DOCA0141ZH-03

ComPact NSX100-250 - 配电保护

MicroLogic 5.26.2 AE7.2 E 脱扣单元

MicroLogic 5.2 6.2AE,以及  7.2E

40–160 A

Reflex 脱扣

MicroLogic 5.2 6.2AE,以及  7.2E

250 A

Reflex 脱扣

MicroLogic  6.2AE(接地故障保护)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

这有帮助吗?