DOCA0213EN-03

Circuit Breaker Status

Circuit Breaker Status

Address

Register

RW

X

Unit

Type

Range

A/E

Bit

Description

0x0232

563

R

INT16U

A/E

Circuit breaker status register

0

OF input status

0 = The circuit breaker is open.

1 = The circuit breaker is closed.

1

SD input status

0 = The circuit breaker is not tripped.

1 = The circuit breaker is tripped due to electrical fault or shunt trip or push-to-trip.

2

SDE input status

0 = The circuit breaker is not tripped on electrical fault.

1 = The circuit breaker is tripped due to electrical fault (including ground-fault test and earth-leakage test).

3–15

Reserved (forced to 0)

Communicating Motor Mechanism Status

Address

Register

RW

X

Unit

Type

Range

A/E

Bit

Description

0x0233

564

R

INT16U

A/E

Communicating motor mechanism status register

0

Motor mechanism

0 = not available

1 = available

1

Manu/auto mode

0 = manu

1 = auto

2

Last command

0 = last command succeeded

1 = last command failed

3

Enable automatic reset

0 = automatic reset is not enabled.

1 = automatic reset is enabled.

4

Enable reset even if SDE

0 = reset is not enabled if the circuit breaker is tripped on electrical fault.

1 = reset is enabled even if the circuit breaker is tripped on electrical fault.

5

Local/Remote mode selected in the FDM121 display menu.

0 = Remote mode (default value), the communicating motor mechanism is controlled through a Modbus command only.

1 = Local mode, the communicating motor mechanism is controlled through the FDM121 display menu only.

6–15

Reserved (forced to 0)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.