DOCA0213EN-03

Description

Modbus Communication

The Modbus communication option enables Schneider Electric low voltage circuit breakers to be connected to a supervisor or to any other device with a Modbus client communication channel.

The circuit breakers can be connected to:

  • An RS-485 serial line network with Modbus protocol using dedicated interfaces such as:

    • The BSCM Modbus SL/ULP module and the Modbus SL hub.

    • The IFM Modbus SL communication interface for one circuit breaker.

  • An Ethernet network with Modbus TCP/IP protocol using dedicated interfaces such as:

    • The IFE Ethernet communication interface for one circuit breaker.

    • The IFE Ethernet switchboard server.

Access to Functions

The Modbus communication option provides access to many functions, including:

  • Read metering and diagnostic data

  • Read status conditions and remote operations

  • Transfer of time-stamped events

  • Display protection settings

  • Read the circuit breakers identification and configuration data

  • Remote control of the circuit breaker

  • Time-setting and synchronization

This list depends on the composition of the intelligent modular unit (IMU) (type of circuit breaker, of MicroLogic trip unit, and so on) and the enabled functions.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.