0000509775_02_en

Configure the Webmanager

The webmanager needs to be configured for the specific battery setup. The webmanager interface is accessed locally or remotely through a connected network. From the webmanager interface the modules must be programed with a unique address for each module on the bus.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?