DOCA0178EN-22

New Features for Firmware Version 002.003.000

  • Security improvements in EcoStruxure Panel Server:

    • Security patch

  • Addition of support for a Modbus serial device associated with multiple meters. The meters must share the same Unit ID and must be added using custom models. For example, the Rayleigh multi-circuit meter can be configured as:

    • Either 2 three-phase circuits, using 2 dedicated custom models

    • Or 6 single-phase circuits, using 6 dedicated custom models

    The 2 or 6 circuits are added manually to the Panel Server as Modbus devices at Settings > Modbus devices > Modbus TCP/IP > Manual addition, using a specific custom model for each circuit. The 2 or 6 devices must share the same:

    • Unit ID

    • IP address

    • Port

  • Introduced logic code INT64ToFloat32 to convert INT64 values to Float32 values.

  • The following obsolete Modbus built-in device models are no longer supported:

    • apas

    • bpas

    • bcpm a

    • bcpm b

    • bcpm c

    • masterpact_nt_nw_a (MasterPacT NT/NW with MicroLogic A connected directly to BCM ULP serial line without IFE/IFM interface)

    • masterpact_nt_nw_e (MasterPacT NT/NW with MicroLogic E connected directly to BCM ULP serial line without IFE/IFM interface)

    • masterpact_nt_nw_h (MasterPacT NT/NW with MicroLogic H connected directly to BCM ULP serial line without IFE/IFM interface)

    • masterpact_nt_nw_p (MasterPacT NT/NW with MicroLogic P connected directly to BCM ULP serial line without IFE/IFM interface)

    Devices associated with these obsolete models are henceforth listed as unknown devices. Historized alarms are retained.

    If you use these device models, export associated data before updating the Panel Server firmware. After the firmware update, remove the unknown devices and add them manually by creating a custom device model, or by using an existing built-in model. Refer to the list of supported circuit breakers and associated trip units.

  • The following measurements associated with MasterPacT MTZ devices no longer supported:

    • Circuit breaker total durability

    • Circuit breaker service life loaded wear ratio

    • Number of operations with load > 0

    • Circuit breaker service life wear ratio (with and without load)

  • Management of measurements from MasterPacT MTZ circuit breakers connected through IFE, EIFE or IFM interfaces. Update the interface to the latest supported version to ensure correct display of data:

    • For IFE and EIFE interfaces, update the interface to firmware version 003.009.010 or later

    • For IFM interfaces, update the interface to firmware version 003.001.010 or later

  • Additional Modbus settings are available for Modbus registers via Modbus address 255. The following parameters can be consulted:

    • Modbus TCP/IP server settings:

      • Message timeout Modbus TCP/IP server)

    • Modbus TCP/IP client settings:

      • Timeout of Modbus TCP/IP client

      • Message timeout of Modbus TCP/IP client request

    • Modbus SL settings for downstream communication:

      • Silent interval after Modbus SL packet end

      • Delay between Modbus SL packets

      • Connect/Disconnect the RS485 termination resistor

      • Transmission line state

    • Modbus SL client settings

      • Message timeout of Modbus SL request

  • For Panel Server embedded digital inputs configured as Pulse counter, Water volume and Gas volume can be displayed and published with Float32 Modbus registers to improve precision to three decimal places. Existing INT64 Modbus registers are also available. For more information, refer to DOCA0241EN EcoStruxure Panel Server - Modbus File.

New Supported Wireless Devices

  • The following references of PowerLogic Thermal Tag wireless temperature sensors

    • SPTH150S self-powered wireless thermal sensor

    • SPTH150M self-powered wireless thermal sensor with 3 probes

    • SPTH200M wireless thermal sensor with 4 probes

  • The following references of Acti9 Active iCV40H ARC without overvoltage protection alarm:

    • A9TDNC606

    • A9TDNC610

    • A9TDNC616

    • A9TDNC625

    • A9TDNC632

    • A9TDNC640

    • A9TDND606

    • A9TDND610

    • A9TDND616

    • A9TDND620

    • A9TDND625

    • A9TDND632

New Supported Modbus Devices

  • The following references of PowerLogic EM3100, EM3200, EM3300, EM3400 and EM3700 energy meters. The devices can be discovered by the Panel Server using the built-in device model em3000:

    • METSEEM3122

    • METSEEM3224

    • METSEEM3322

    • METSEEM3424

    • METSEEM3724

User Interface Improvements

  • Improved user experience in device pages by adding icon to collapse left pane (device tree) to maximize screen space.

  • Improved webpage header with reorganization of Service status display. Drop down list of services in page header gives summary of the status via an icon , and a link to the Settings page of each service.

  • In Settings > Modbus devices > Device addition > Manual addition, added search function in the Device list to facilitate device search.

  • In Monitoring & Control > Multi device view, Device range information added to overview for improved context.

  • Improved user experience in Settings > Wireless devices > Discovery by adding text to clarify use of discovery methods.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.