DOCA0178EN-22

New Features for Version 002.001.000

  • New model PAS600P released with hardware version 002.000.000

  • Support for the following commands from cloud to Exiway Link devices

    • Locate an Exiway Link device to make it blink for five minutes

    • Disable or enable periodic tests

    • Start functional test

    • Switch light on or off

    • Synchronize Exiway Link devices

  • Addition of the following commands from webpages to Exiway Link devices:

    • Locate an Exiway Link device to make it blink for five minutes

    • Disable or enable periodic tests

    • Start functional test

  • Addition of sampling and publication of following real-time environmental measurements, depending on device connected:

    • Battery voltage

    • Internal temperature

    • RSSI link

Panel Server webpage user experience improvements:

  • Monitoring and Control page organized with two views:

    • Device view: device-centric view allows you to display data for one device. Data is displayed as widgets for each data type.

    • Multi-device view: select up to 5 devices and 2 data types to display. The selection is maintained when clicking away and returning. A link on each device name displays the device view directly.

  • Addition of alarm severity in Data management page for individual devices.

  • Wireless device connection status indicator: added connection status in orange for reduced connection quality with possible loss of communication.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.