DOCA0178EN-22

Firmware Version 001.005.001

New Features

  • Automatic discovery of wireless devices connected under a child gateway (Panel Server, PowerTag Link, or Smartlink SIB).

  • Smartlink SIB gateway natively supported as a child gateway of Panel Server.

  • Defining end-device energy by using the Panel Server webpages (Commodity field in the end-device details, field not published in Schneider Electric cloud services).

  • For any type of PowerTag wireless devices, delivered and received energy available in Modbus registers (upload the most recent version of DOCA0241EN EcoStruxure Panel Server - Modbus File).

  • Publication to SFTP server of data sampled on devices connected to the Panel Server, including authentication to SFTP server with either user name and password or user name and SSH key.

  • Setting of the pulse counter type digital inputs by using the Panel Server webpages.

General Features

The following table presents the availability of general features on EcoStruxure Panel Server Universal in firmware version 001.005.001.

Available

Not available

General features

Availability

Functionality

Separated network topology

Switched network topology

Connection to Edge Control (EcoStruxure Power Monitoring Expert, EcoStruxure Power Operation,EcoStruxure Building Operation, any Building Management System, or third-party monitoring or supervision system)

Ability to disable concurrently and permanently the wireless networks (Wi-Fi and IEEE 802.15.4) by using Panel Server webpages

Wi-Fi

2.4 GHz

External Wi-Fi antenna (reference: PASA-ANT1)

IEEE 802.15.4 communication

Maximum number of wireless devices:

  • Up to 40 wireless devices as combination of PowerTag Energy sensors, PowerLogic Tag energy sensors, Acti9 Active, wireless indication auxiliaries for ComPacT and PowerPacT circuit breakers, wireless CO2 sensors, wireless temperature and humidity sensors, PowerTag A, PowerTag Ambient, Easergy TH110/CL110 environmental sensors, and PowerLogic HeatTag sensors

  • or up to 65 Easergy TH110/CL110 environmental sensors

Modbus TCP/IP communication

64 Modbus TCP/IP devices maximum including devices physically connected to the Panel Server and virtual devices (that is, IEEE 802.15.4 devices connected to a child Panel Server gateway)

Human Machine Interface (HMI)

FDM128 Ethernet display

PowerTag Link display

Backup restore

Backup and Panel Server configuration restore by using Panel Server webpages and EcoStruxure Power Commission software

Configuration

User management by single user account

User management by multiple users with Role-Based Access Control (RBAC)

Alarms

Publication of alarms related to:

  • Communication issue between a device and Panel Server when available from the end devices

  • ERMS on circuit breaker

  • The three levels of alarms from HeatTag sensors

Protocols

Modbus TCP/IP server

Modbus TCP/IP client

DHCP client

DHCP server

DPWS server

HTTPS

SFTP client

Data export

Panel Server webpages for publication on SFTP server

Publication on Schneider Electric cloud by using Panel Server webpages

Commissioning and Monitoring Features

The following table presents the availability of commissioning and monitoring features on EcoStruxure Panel Server Universal in firmware version 001.005.001.

Available

Not available

Commissioning and monitoring features

Availability

Modbus serial communication

Commissioning of feature to use the Modbus serial port in reverse mode by using Panel Server webpages

Digital inputs (PAS600L)

Commissioning by using EcoStruxure Power Commission software

Commissioning by using Panel Server webpages

Monitoring by using EcoStruxure Power Commission software

Monitoring by using Panel Server webpages

Firmware update

Applied to one Panel Server gateway by using EcoStruxure Power Commission software

Applied to one Panel Server gateway by using Panel Server webpages

Applied to several Panel Server gateways by using EcoStruxure Power Commission software

Applied to several Panel Server gateways by using Panel Server webpages

Backup restore

Backup restore on a Panel Server of the same model by using EcoStruxure Power Commission software

Backup restore on a Panel Server of the same model by using Panel Server webpages

Configuration

Configuration by using EcoStruxure Power Commission software

Ethernet configuration for upstream communication by using Panel Server webpages

Modbus configuration of Modbus TCP/IP and Modbus serial devices by using Panel Server webpages

Selective pairing of wireless devices by using EcoStruxure Power Commission software

Selective pairing of wireless devices by using Panel Server webpages

Disable concurrently and permanently the wireless networks (Wi-Fi and IEEE 802.15.4) in the Panel Server by using Panel Server webpages

Monitoring

Display of data of Smartlink Modbus devices by using Panel Server webpages

Display of data of Panel Server digital inputs by using Panel Server webpages

Display of data of the supported devices (see commercial references in Supported Devices) by using Panel Server webpages

Diagnostic by using Panel Server webpages

Performance and Limitations

  • Performance and limitations on Panel Server Universal:

    • When SFTP publication is enabled, alarms are displayed in the Panel Server webpages but are not published on SFTP Server.

    • No manual addition of wireless devices connected to a child/downstream gateway by using EcoStruxure Power Commission software.

    • Automatic discovery of wireless devices under a child gateway is limited to 64 devices because wireless devices are seen as Modbus TCP/IP devices.

    • The typical response time to Modbus TCP/IP request for a wireless IEEE 802.15.4 device is 30 ms.

    • The maximum response time to Modbus TCP/IP request for a wireless IEEE 802.15.4 device is 1 s, set up Modbus/TCP client timeout accordingly.

    • Typical Panel Server latency between Modbus TCP/IP request forwarded to the Modbus serial network is 10 ms.

    • Wi-Fi function available through a connection to a Wi-Fi infrastructure only. Access point function not available.

  • Limitations on sampling and publishing for cloud applications:

    • The number of individual data points that can be sampled is limited to 2,000 and limited to a flow of 500 data points per minute.

    • The number of individual alarms that can be configured for monitoring is limited to 100.

  • Limitations on Smartlink Modbus:

    • Commissioning by using EcoStruxure Power Commission software only (not available through Panel Server webpages).

    • Control of Smartlink Modbus output(s) by using Panel Server webpages is not available.

  • Limitations on wireless devices: PowerTag Control and PowerTag Display are not supported by Panel Server Universal.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.