DOCA0178EN-22

Major Fixes for Firmware Version 002.004.000

  • Wireless devices were intermittently unable to perform a command sent from the Panel Server and the message Action already in progress was displayed in the webpages.

  • A remote configuration was not applied successfully if some Modbus devices experienced communication issues with the Panel Server at the moment that the remote configuration was received from the Cloud. The Last remote configuration status may be indicated as Reset to blank state.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.