DOCA0178EN-22

Firmware Update with EcoStruxure Panel Server Webpages

To update the firmware with the Panel Server webpages, proceed as follows:

  1. Make sure that the Panel Server is continuously powered during the firmware update.

  2. Retrieve the latest version of Panel Server firmware and save on your PC in one of the following ways:

    • From your Schneider Electric country website

      NOTE: Ensure that you select the firmware update suitable for your Panel Server model and hardware version.
    • Directly from the Maintenance > Firmware update page of the webpages in step 5 of this procedure. The correct firmware update suitable for your Panel Server model is automatically selected.

  3. Connect your PC to the Panel Server via an Ethernet cable or via Wi-Fi through the Wi-Fi access point.. The connection procedures are described in DOCA0172•• EcoStruxure Panel Server - User Guide.

  4. Follow the procedure described in DOCA0172•• EcoStruxure Panel Server - User Guide to access the Panel Server webpages.

  5. From the Panel Server webpages, navigate to Maintenance > Firmware update. You can download the correct firmware update from the section Retrieve the appropriate firmware. Click Download file to download it to your PC.

  6. In the Firmware update section, import the firmware file by clicking Import file and selecting the downloaded firmware file from your file explorer. Follow the on-screen instructions.

  7. Reboot the Panel Server to update the firmware.

    NOTE: The Panel Server webpages cannot be accessed while the Panel Server is rebooting.

  8. After the reboot, check that the firmware version is the latest to make sure that the update is effective.

    If the firmware version is still the old one, perform the firmware update procedure again.

    If the problem persists, contact your Schneider Electric customer support.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.