DOCA0178EN-22

Commissioning and Monitoring Features

The following table presents the availability of commissioning and monitoring features on Panel Server Universal in firmware version 002.006.001.

Available

Not available

Commissioning and monitoring features

Availability

Modbus serial communication

Commissioning of feature to use the Modbus serial port in reverse mode by using Panel Server webpages

Digital inputs (PAS600L, PAS600LWD)

Commissioning by using EcoStruxure Power Commission software

Commissioning by using Panel Server webpages

Monitoring by using EcoStruxure Power Commission software

Monitoring by using Panel Server webpages

Status assignment from a list of predefined values for each generic input/output in the I/O contextualization setting by using EcoStruxure Power Commission software or Panel Server webpages

Firmware update

Applied to one Panel Server gateway by using EcoStruxure Power Commission software

Applied to one Panel Server gateway by using Panel Server webpages

Applied to several Panel Server gateways by using EcoStruxure Power Commission software

Applied to several Panel Server gateways by using Panel Server webpages

Backup and restore

Backup and restore on a Panel Server of the same model by using EcoStruxure Power Commission software

Backup and restore on a Panel Server of the same model by using Panel Server webpages

Configuration

Configuration by using EcoStruxure Power Commission software

Ethernet configuration for upstream communication by using Panel Server webpages

Wi-Fi configuration for upstream communication by using Panel Server webpages

Modbus configuration of Modbus TCP/IP and Modbus serial devices by using Panel Server webpages

Selective discovery of wireless devices by using EcoStruxure Power Commission software

Selective discovery of wireless devices by using Panel Server webpages

Automatic discovery of wireless devices by using Panel Server webpages

Disable concurrently and permanently the wireless networks (Wi-Fi and IEEE 802.15.4) in the Panel Server by using Panel Server webpages

Monitoring

Display of data of I/O Smart Link devices by using Panel Server webpages

Display of data of Panel Server digital inputs by using Panel Server webpages

Display of data of the supported devices (see commercial references in Supported Devices) by using Panel Server webpages

Diagnostic by using Panel Server webpages

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.