General Features
The following table presents the availability of general features on Panel Server Universal in firmware version 002.006.001.
● Available
● Not available
|
General features |
Availability |
||
|---|---|---|---|
|
Functionality |
Separated network topology |
● |
|
|
Switched network topology |
● |
||
|
Connection to Edge Control (EcoStruxure Power Monitoring Expert, EcoStruxure Power Operation,EcoStruxure Building Operation, any Building Management System, or third-party monitoring or supervision system) |
● |
||
|
Ability to disable concurrently and permanently the wireless networks (Wi-Fi and IEEE 802.15.4) by using Panel Server webpages |
● |
||
|
Wi-Fi |
2.4 GHz |
● |
|
|
5 GHz (hardware version 002.000.000) |
● |
||
|
External Wi-Fi antenna (reference: PASA-ANT1) |
● |
||
|
Wi-Fi access point, available to connect a smartphone running the Schneider Electric EcoStruxure Power Commission mobile app |
● |
||
|
Human Machine Interface (HMI) |
FDM128 Ethernet display |
● |
|
|
Configuration |
User management by single user account |
● |
|
|
User management by multiple users with Role-Based Access Control (RBAC) |
● |
||
|
Alarms |
|
● |
|
|
Protocols |
IEEE 802.15.4 |
● |
|
|
Modbus TCP/IP server |
● |
||
|
Modbus TCP/IP client |
● |
||
|
DHCP client |
● |
||
|
DHCP server |
● |
||
|
DPWS server |
● |
||
|
HTTPS |
● |
||
|
SFTP client |
● |
||
|
RSTP |
● |
||
|
Data export |
Panel Server webpages for publication on SFTP server or HTTPS server |
● |
|
Publication on Schneider Electric cloud by using Panel Server webpages |
● |
Maximum Configuration
The maximum number of devices that can be configured in a system with a Panel Server Universal depends on the type of connected devices:
| Device type |
Maximum number of concurrent devices |
|
|---|---|---|
|
Wireless device (not supported by PAS600LWD and PAS600PWD) |
PowerTag Energy sensors |
85 |
|
PowerLogic Tag energy sensors |
85 |
|
|
Acti9 Active devices |
85 |
|
|
Wireless indication auxiliaries for ComPacT and PowerPacT circuit breakers |
85 |
|
|
MasterPacT MTZ circuit breakers with MicroLogic Active AP or EP control unit |
8 |
|
|
Wireless CO2 sensors |
100 |
|
|
Wireless temperature and humidity sensors |
100 |
|
|
PowerTag Ambient sensors |
100 |
|
|
PowerLogic TH110/CL110 environmental sensors |
100 |
|
|
PowerLogic Thermal Tag TH150/TH200 wireless temperature sensors |
100 |
|
|
PowerLogic HeatTag sensors |
15 |
|
|
PowerTag Control devices |
10 |
|
|
PowerLogic PD100 devices |
15 |
|
|
Exiway Link devices |
20 |
|
|
XB5R transmitters (ZBRT) |
100 |
|
|
The recommendation for a mixed configuration of wireless devices is as follows:
|
||
|
Modbus-SL devices |
Modbus-SL devices other than I/O devices: |
32 NOTE: The maximum number depends on the serial line length
and the type of device(s).
|
|
I/O devices:
|
|
|
|
Modbus TCP/IP devices |
Devices physically connected to the Panel Server and virtual devices, that is, IEEE 802.15.4 wireless devices connected to a child Panel Server gateway. |
128 NOTE: The Panel Server supports 64 simultaneous Modbus TCP/IP client connections (for
example, SCADA system).
|