DOCA0178EN-22

New Features for 002.002.000

  • Security improvements in Panel Server:

    • Password policy reinforced with new rules. Follow the new rules from your next password update. For more information about Password Requirements, refer to DOCA0172•• EcoStruxure Panel Server - User Guide.

    • Protect Plus: Install code introduced for discovery with heightened security of 16-character RF-ID wireless devices.

  • Wi-Fi access point allows you to use a PC to connect to the Wi-Fi network of the Panel Server, providing access to Panel Server webpages for device configuration, monitoring and firmware update.

  • Custom models can now include the Modbus discovery rules, which allows the Panel Server to use custom models in addition to built-in models to discover Modbus devices, without the need to use manual addition.

  • New supported devices: XB5R transmitters: ZBRT1 and ZBRT2. For more information about adding and removing ZBRT devices, refer to DOCA0172•• EcoStruxure Panel Server - User Guide.

  • Support for new measurements for motor controller devices:

    • Pole state

    • Contactor state

    • Speed setpoint

    • Motor speed

    • Direction of motor rotation

  • Introduction of maximum number of 50 custom models imported to Panel Server. Each model can have one current version and one available version.

User Interface Improvements

  • Monitoring & Control webpage:

    • Devices sorted by alphabetical usage in tree view. Devices with no usage assigned are displayed in a No usage category, at the end of the list. Each usage can be collapsed to improve clarity of display.

    • Width of first column is reduced in multi-device view to improve display.

    • A new data type Health state can be selected for display in multi-device view, with the following data:

      • Battery voltage

      • Internal temperature

      • RSSI link

  • Data management webpage: Devices are sorted by alphabetical usage in tree view. Devices with no usage assigned are displayed in a No usage category, at the end of the list. Each usage can be collapsed to improve clarity of display.

  • RF-ID of device is displayed in Settings > Wireless devices in the header for each wireless device

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.