DOCA0178EN-22

About the Document

Document Scope

This document provides users with the following information about the EcoStruxure™ Panel Server Universal gateway:

  • New features, major fixes, and limitations for the latest firmware version

  • List of supported devices

  • History of previous firmware versions

Validity Note

This document applies to the Panel Server Universal gateway with firmware version 002.006.001.

Online Information

The characteristics of the products described in this document are intended to match the characteristics that are available on www.se.com. As part of our corporate strategy for constant improvement, we may revise the content over time to enhance clarity and accuracy. If you see a difference between the characteristics in this document and the characteristics on www.se.com, consider www.se.com to contain the latest information.

General Cybersecurity Information

In recent years, the growing number of networked machines and production plants has seen a corresponding increase in the potential for cyber threats, such as unauthorized access, data breaches, and operational disruptions. You must, therefore, consider all possible cybersecurity measures to help protect assets and systems against such threats.

To help keep your Schneider Electric products secure and protected, it is in your best interest to implement the cybersecurity best practices as described in the Cybersecurity Best Practices document.

Schneider Electric provides additional information and assistance:

Available Languages of the Document

The document is available in these languages:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.