DOCA0178EN-22

Limitations for Firmware Version 002.005.000

General Performance and Limitations

  • Keep firmware up to date in order to allow the Schneider Electric Customer Care Center to remotely access the Panel Server webpages.

    Remote access certificates for each firmware version are valid up to the dates indicated in the table.

    Panel Server firmware version Remote access certificate validity date

    002.005.000

    08 October 2026

    002.004.000

    10 August 2026

    002.003.000

    07 May 2026

    For more information about Firmware Update, refer to DOCA0172•• EcoStruxure Panel Server - User Guide.

Limitations on Wireless Devices

  • Under certain circumstances, after a restore operation on Panel Server, the Settings page for a PowerTag Control IO device (A9XMC1D3) may be inaccessible on Panel Server webpages. The page remains in a loading loop and does not display the configuration settings. The PowerTag Control IO device continues to function correctly.

    Contact Schneider Electric Customer Care Center to restore access to the configuration page for this device.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.