DOCA0178EN-22

New Features for 002.000.000

  • Increase in the maximum number of alarms that can be selected for publication from 100 to 500. Among the 500 alarms, a maximum of 300 can be from Modbus-SL devices.

  • Addition of the following supported devices:

    • Wireless devices:

      • Exiway Light device

      • MasterPacT MTZ with MicroLogic Active AP or EP

    • Modbus devices: BSCM Modbus SL/ULP module

  • Wi-Fi access point enables you to connect to the Wi-Fi network of the Panel Server from a smartphone running the Schneider Electric EcoStruxure Power Commission mobile app . From the app you can configure connected devices.

  • Addition of local time zone which can be set at Settings > General > Date and time. When set, the local time zone is used:

    • For data displayed on the Monitoring & Control webpage

    • In emails for alarms

    • For data published to an SFTP or HTTPS server

    • For data exported in a local file

    UTC is used to publish to cloud applications and for logging data, even when local time zone is set.

  • Addition of support for RSTP protocol allowing robust Ethernet ring topologies for critical applications. RSTP is available only when the Panel Server is configured in switched mode.

  • Addition of the following supported measurements:

    • Steam volume (m3)

    • Steam flow (m3/s)

    • Steam mass flow (kg/s)

    • Air volume (m3)

    • Air flow (m3/s)

    These measurements are specified in a custom device model created in the EcoStruxure Power Commission web portal tool and imported into the Panel Server. The measurement values are available in the Monitoring & Control webpage.

  • Panel Server webpage user experience improvements:

    • Loading time of webpages improved.

    • Data management page improvements:

      • A banner message gives information about the purpose and result of selecting measurements and alarms.

      • Date and time of last measurement data update is displayed at the top of the page.

    • In Monitoring & Control webpage, addition of date and time of last measurement data update at the top of the page.

    • In Maintenance > Firmware update page, addition of following sections:

      • Retrieve the correct firmware with button to click to allow you to download the correct firmware update for your Panel Server directly to your PC.

      • Further information with button to click to allow you to access general information related to Panel Server products.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.