DOCA0178EN-22

Firmware Version 001.003.001

New Features

  • Addition of EcoStruxure Panel Server webpages for monitoring

  • Enhancement of response time to Modbus TCP/IP request and operation for a wireless IEEE 802.15.4 device

  • Addition of alarms for PowerTag and PowerLogic Tag wireless energy sensors:

    • 45% rated current alarm

    • 50% rated current alarm

    • 80% rated current alarm

    • Zero current alarm

  • Wi-Fi infrastructure mode using internal antenna or external antenna (reference PASA-ANT1).

  • Manual addition of Modbus Serial devices connected to a child/downstream gateway. For example, child/downstream gateways can be Panel Server, Link150 or third-party gateways.

    Example: Two Modbus Serial devices are connected to a child/downstream Panel Server in a separate topology. The child/downstream Panel Server (PAS#2) is connected to one Ethernet port of the parent/upstream Panel Server (PAS#1). For more information, refer to DOCA0172EN EcoStruxure Panel Server - User Guide.

  • Integration with Schneider Electric cloud applications EcoStruxure Asset Advisor, EcoStruxure Resource Advisor, and EcoStruxure Energy Hub with limited features. For more information, contact your local Schneider Electric representative.

  • Ethernet diagnostics to help with validating the Panel Server integration into upstream communication.

  • New languages supported in EcoStruxure Panel Server webpages: Italian, Spanish, German, Russian.

  • For wireless devices, configuration of communication period per family (energy, ambient, control) on EcoStruxure Panel Server webpages and EcoStruxure Power Commission software.

  • FDM128 display supported but need to update to last version of FDM128 firmware (version 8.0.30 or higher). For detailed information about supported wireless devices, refer to DOCA0151EN Enerlin'X FDM128 – Ethernet Display for Eight Devices – Firmware Release Notes.

    Acti9 Active, wireless indication auxiliaries for ComPacT and PowerPacT, and PowerLogic Tag are not displayed.

  • Remote access (a local action is required to enable remote access to the EcoStruxure Panel Server webpages).

Known Issues

EcoStruxure Power Commission software version 2.24 does not use virtual server ID to access Modbus Serial devices.

When a virtual server ID different from the physical Modbus address / server ID is allocated to a Modbus Serial device, EcoStruxure Power Commission software version 2.24 uses the physical Modbus address / server ID to access the Modbus Serial device.

To avoid any issue during commissioning of Modbus Serial devices in EcoStruxure Power Commission software, ensure that the physical Modbus address / server ID and the virtual server ID of each downstream Modbus device under the Panel Server gateway are unique and have not been previously assigned as a physical Modbus address or virtual server ID to any wireless, Modbus Serial, or Modbus TCP/IP device.

To solve this issue, proceed as follows:

  • Option 1 - Change the physical Modbus address of the device on the Modbus Serial network as follows:

    1. Set the physical Modbus address of the device to a value not assigned as virtual server ID to any other wireless, Modbus Serial, or Modbus TCP/IP device.

    2. Login to the Panel Server webpages and update accordingly the physical Modbus address / server ID of the device in the Panel Server.

  • Option 2 - Change the virtual server ID of the device in the Panel Server as follows:

    Login to the Panel Server webpages and change the virtual server ID of the device to a value different from the physical Modbus address / server ID of any other device on the Modbus Serial network.

Issues Fixed

All known issues in firmware version 001.002.000 are fixed.

Features

The following table presents the availability of features on EcoStruxure Panel Server Universal in firmware version 001.003.001.

Available

Not available

Features

Availability

Functionality

Separated network topology

Switched network topology

Connection to Edge Control (EcoStruxure Power Monitoring Expert, EcoStruxure Power Operation,EcoStruxure Building Operation, any Building Management System, or third-party monitoring or supervision system)

Embedded webpages for diagnostic

Embedded webpages for monitoring all the supported devices (see commercial references in Supported Devices).

Wi-Fi

2.4 GHz

External Wi-Fi antenna (reference: PASA-ANT1)

IEEE 802.15.4 communication

Maximum number of wireless devices:

  • Up to 30 wireless devices as combination of PowerTag Energy sensors, PowerLogic Tag energy sensors, Acti9 Active, wireless indication auxiliaries for ComPacT and PowerPacT circuit breakers, wireless CO2 sensors, wireless temperature and humidity sensors, PowerTag A, PowerTag Ambient, environmental sensors Easergy TH110/CL110, and PowerLogic HeatTag sensors, with a maximum of:

    • 20 PowerTag or PowerLogic Tag energy sensors, or Acti9 Active

    • 3 PowerLogic HeatTag

    • 6 wireless indication auxiliaries for ComPacT and PowerPacT circuit breakers

  • or up to 65 environmental sensors Easergy TH110/CL110

Digital inputs (PAS600L)

Commissioning with EcoStruxure Power Commission software

Commissioning with EcoStruxure Panel Server webpages

Monitoring with EcoStruxure Power Commission software and EcoStruxure Panel Server webpages

Human Machine Interface (HMI)

FDM128 Ethernet display

PowerTag Link display

Configuration

EcoStruxure Power Commission software

Embedded webpages for Ethernet settings for upstream communication

Embedded webpages for Modbus settings of Modbus TCP/IP and Modbus Serial devices

User management by single user account

User management by multiple users with Role-Based Access Control (RBAC)

Protocols

Modbus TCP/IP server

Modbus TCP/IP client

DHCP client

DHCP server

DPWS

HTTPS

Performance and Limitations

  • Performance and limitations on EcoStruxure Panel Server Universal:

    • Function to backup and restore Panel Server configuration not available.

    • Alarms not set and not displayed in EcoStruxure Panel Server webpages.

    • No capability to collect data from a wireless end device connected to a child/downstream gateway of the Panel Server such as another Panel Server, a PowerTag Link, or a Smartlink SIB gateway).

    • The typical response time to Modbus TCP/IP request for a wireless IEEE 802.15.4 device is 30 ms.

    • The maximum response time to Modbus TCP/IP request for a wireless IEEE 802.15.4 device is 1 s, set up Modbus/TCP client time-out accordingly.

    • Typical Panel Server latency between Modbus TCP/IP request forwarded to the Modbus RS485 network is 10 ms.

    • Wi-Fi function available through a connection to a Wi-Fi infrastructure only. Access point function not available.

  • Limitations on Smartlink Modbus:

    • Commissioning through EcoStruxure Power Commission software, not through EcoStruxure Panel Server webpages.

    • Status of Smartlink Modbus inputs/outputs or counter available from the Modbus registers, not displayed on EcoStruxure Panel Server webpages.

    • Alarms not displayed in EcoStruxure Panel Server webpages.

    • No control of Smartlink Modbus through EcoStruxure Panel Server webpages.

  • Limitations on wireless devices: PowerTag Control are not supported by EcoStruxure Panel Server Universal.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.