DOCA0178EN-22

Major Fixes for Version 002.001.000

The following bugs are fixed in Panel Server firmware version 002.001.000:

  • Wi-Fi signal strength icon on Panel Server webpage Wi-Fi infrastructure did not display correct signal strength.

  • Acti9 Active devices blocked the publication of the Panel Server topology.

  • Power meter models PM5340 and PM5341 displayed as unknown devices when discovered by the Panel Server.

  • Certain special characters were not accepted in the password when connecting to the SFTP server or the HTTPS server.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.