DOCA0178EN-22

Firmware Version 001.002.000

New Features

  • Addition of supported devices:

    • HeatTag sensors

    • Wireless indication auxiliaries for ComPacT and PowerPacT circuit breakers

    • PowerLogic Tag 2P energy sensors

    • Wireless CO2 sensors

    • Wireless temperature and humidity sensors

    • PowerTag A (EwSenseTemp) sensor

    • PowerTag Ambient wireless temperature sensors

  • Addition of separated network topology

  • Addition of Modbus TCP/IP client protocol

  • Addition of digital inputs to monitor the state of external contacts or as pulse counter

  • Addition of EcoStruxure Panel Server webpages for monitoring

  • Enhancement of typical response time to Modbus/TCP IP request for a wireless IEEE 802.15.4 device

  • Enhancement of maximum response time to Modbus/TCP IP request for a wireless IEEE 802.15.4 device

Known Issues

  • The separated mode is configured to segregate downstream Modbus TCP/IP devices connected on ETH1 port from upstream communication systems connected on ETH2 port. With the current firmware version, it is only possible to access the downstream Modbus TCP/IP devices data from the EcoStruxure Panel Server embedded webpages. A monitoring software connected on ETH1 port using Modbus TCP/IP will not be able to access the Modbus TCP/IP devices connected on ETH2 port. For such applications, use only the switched mode.

  • When an active alarm is present (as reported in the Modbus register) for a PowerTag Energy M250/M630 for ComPacT NSX 3-pole circuit breaker, a PowerTag Energy F160, a PowerTag Rope, or a PowerLogic Tag Rope (see commercial references in the table below), the alarm is still active although the value of the ENVT (External Neutral Voltage Tap) setting is changed by using the EcoStruxure Panel Server webpages or EcoStruxure Power Commission software.

    To work around this issue, restart the EcoStruxure Panel Server Universal (see DOCA0172EN EcoStruxure Panel Server - User Guide for detailed procedure).

    The alarm for phase-to-neutral voltage protection is one of the following:

    • 80% Undervoltage on phase-to-neutral

    • 120% Overvoltage on phase-to-neutral

    The following table lists the devices concerned by the issue:

    Devices

    Commercial reference

    PowerTag M250 3P 250A

    LV434020

    PowerTag M250 3P+N 250A

    LV434021

    PowerTag M630 3P 630A

    LV434022

    PowerTag M630 3P+N 630A

    LV434023

    PowerTag F160 3P/3P+N

    A9MEM1580

    PowerTag Rope 200 A 3P/3P+N

    A9MEM1590

    PowerTag Rope 600 A 3P/3P+N

    A9MEM1591

    PowerTag Rope 1000 A 3P/3P+N

    A9MEM1592

    PowerTag Rope 2000 A 3P/3P+N

    A9MEM1593

    PowerLogic Tag Rope 120A 3P

    PLTR1203P

    PowerLogic Tag Rope 600A 3P

    PLTR6003P

    PowerLogic Tag Rope 1000A 3P

    PLTR10003P

    PowerLogic Tag Rope 2000A 3P

    PLTR20003P

  • When an active alarm is present (as reported in the Modbus register) for a PowerTag Energy 1P+N , a PowerLogic Tag 1 P or 2P, or an Acti9 Active iC40 or iC60, the alarm is still active although the value of the Phase Sequence setting is changed by using the EcoStruxure Panel Server webpages or EcoStruxure Power Commission software.

    To work around this issue, restart the EcoStruxure Panel Server Universal (see DOCA0172EN EcoStruxure Panel Server - User Guide for detailed procedure).

    The alarm about phase sequence is one of the following:
    • 80% Undervoltage

    • 120% Overvoltage

    • Overcurrent over 45%, 50%, or 80% of nominal current

    • Load current is 0 A

    The following table lists the devices concerned by the issue:

    Devices

    Commercial reference

    PowerTag A9 P63 1P+N Top

    A9MEM1560

    PowerTag A9 P63 1P+N Top

    A9MEM1561

    PowerTag A9 P63 1P+N Bottom

    A9MEM1562

    PowerTag A9 P63 1P+N Bottom RCBO

    A9MEM1563

    PowerTag A9 F63 1P+N 110V

    A9MEM1564

    PowerLogic Tag QO 10-30A 1P+N

    PLTQO301P

    PowerLogic Tag QO 35-60A 1P+N

    PLTQO601P

    PowerLogic Tag E-Frame 10-60A 1P+N

    PLTE601P

    PowerLogic Tag QO 10-30A 2P

    PLTQO302P

    PowerLogic Tag QO 35-60A 2P

    PLTQO602P

    PowerLogic Tag E-Frame 10-60A 2P

    PLTE602P

    Acti9 Active iC40 and iC60 A9TAA●●●●, A9TAB●●●●, A9TDEC●●●, A9TDFC●●●, A9TDFD●●●, A9TPDD●●●, A9TPED●●●, A9TYAE●●●, A9TYBE●●●
  • On systems with both Modbus devices and wireless devices, the table view of measurements may display in some rare cases the same measurements value for the wireless devices as for the Modbus device as shown below:

    This issue is only within this page and does not affect the measurements reported on the Modbus register to the upstream system nor the measurements reported in the single device webpage.

    This issue does not affect systems with only wireless devices or only Modbus devices.

    Follow this procedure to resolve the issue:

    • For systems with more wireless devices than Modbus devices (for example, 10 wireless devices and 5 Modbus devices):

    1. Remove all devices from the project.

    2. Add all Modbus devices.

    3. Add all wireless devices.

    4. Remove the wireless devices only again.

    5. Add all the wireless devices again.

    • For systems with more Modbus devices than wireless devices (for example, 10 Modbus devices and 5 wireless devices):

    1. Remove all devices from the project.

    2. Add all wireless devices.

    3. Add all Modbus devices.

    4. Remove the Modbus devices only again.

    5. Add all the Modbus devices.

    • For systems with same number of Modbus devices as wireless devices (for example, 5 Modbus devices and 5 wireless devices):

    1. Remove all devices from the project.

    2. Add all wireless devices.

    3. Add all Modbus devices.

    4. Remove the Modbus devices only again.

    5. Add all the Modbus devices.

Features

The following table presents the availability of features on EcoStruxure Panel Server Universal in firmware version 001.002.000.

Available

Not available

Features

Availability

Functionality

Separated network topology

Switched network topology

Connection to Edge Control (EcoStruxure Power Monitoring Expert, EcoStruxure Power Operation,EcoStruxure Building Operation, any Building Management System, or third-party monitoring or supervision system)

Embedded webpages for diagnostic

Embedded webpages for monitoring all the supported devices (see commercial references in chapter Supported Devices).

Wi-Fi

2.4 GHz

5 GHz

External Wi-Fi antenna

IEEE 802.15.4 communication

Maximum number of wireless devices:

  • Up to 30 wireless devices as combination of PowerTag Energy sensors, PowerLogic Tag energy sensors, Acti9 Active, wireless indication auxiliaries for ComPacT and PowerPacT circuit breakers, wireless CO2 sensors, wireless temperature and humidity sensors, PowerTag A, PowerTag Ambient, environmental sensors Easergy TH110/CL110, and PowerLogic HeatTag sensors, with a maximum of:

    • 20 PowerTag or PowerLogic Tag energy sensors, or Acti9 Active

    • 3 PowerLogic HeatTag

    • 6 wireless indication auxiliaries for ComPacT and PowerPacT circuit breakers

  • or up to 65 environmental sensors Easergy TH110/CL110

Digital inputs

Configuration

EcoStruxure Power Commission software

Embedded webpages for configuration of Ethernet and Modbus settings

User management: single user

Protocols

Modbus TCP/IP server

Modbus TCP/IP client

DHCP client

DHCP server

DPWS

HTTPS

Performances and Limitations

  • The typical response time to Modbus/TCP IP request for a wireless IEEE 802.15.4 device is 30 ms.

  • The maximum response time to Modbus/TCP IP request for a wireless IEEE 802.15.4 device is 1 s, set-up Modbus/TCP client time-out accordingly.

  • Typical EcoStruxure Panel Server latency between Modbus TCP/IP request forwarded to the Modbus RS485 network is 10 ms.

  • The maximum number of Modbus/TCP concurrent connections is 32.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.