DOCA0184EN-07

Modify the Enclosure Features

It is possible to modify the enclosure in the same range by right-clicking within the enclosure:

  • Modify the enclosure characteristics

  • Cancel the enclosure

  • Modify the height

  • Modify the width

It is possible to change the enclosure range by clicking the modify range button on the right side of the screen. The devices which are displayed in the workbench, to be then mounted in the new enclosure.(except for the comb busbar range).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?