DOCA0184EN-05

Front View

The list of the panels in the project is accessible from the electrical diagram and single line diagram page.

To switch to another panel in the project:

  • Click on the name of the panel which is currently displayed.

  • Click on the name of another panel in the list.

QR code for this page

Was this helpful?