DOCA0184EN-07

Select the Enclosure

It is possible to directly select an enclosure range by clicking on the range picture and validate.

To get guidance in selecting a range, set the ratio of modular free space in the panel, set the enclosure characteristics in the proposed list, select a range not marked with an orange mark and validate.

It is required to fine tune the characteristics of the enclosure in the selected range.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?