DUG_Matter Thermostat_ELKO-01

Cybersecurity

Cybersecurity aims to prevent your system, communication networks, and devices from possible attacks, data tampering, or confidential information leakage.

Following these cybersecurity principles may help to reduce the risk of cyber threats to the network where your system is installed.

  • Keep your phone up-to-date and install the latest security updates.

  • Only connect to secure Wi-Fi networks.

  • Only download apps from Google Play or Apple store.

  • Use all the security settings on your smart phone/tablet:

    • Long passcodes or pass phrases

    • Two-factor authentication (2FA)

    • Facial recognition

    • Block unknown apps

Refer CSA Matter Security Principles.

Secure disposal / End of Life / Decommission

If a device needs to be disposed of, perform a factory reset to delete all data, project data, and programming is deleted from the device. Make sure that it is securely disposed to prevent its redeployment into your operational system or unauthorized use.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?