DUG_Matter Thermostat_ELKO-03

Matter system

The thermostat can be commissioned with any Matter compatible smart home system and their respective controllers/hubs for seamless user experience.

System requirement

Before setting up the thermostat in your smart home, you need to make sure that you meet the minimum system requirements.

Smartphone:

  • Apple users: iOS 16.1 or later.

  • Android users: Android 8.1 or later

Connectivity and hub:
Connect Matter device with Wi-Fi® router on 2.4 GHz bands and your preferred smart home platform.

TIP: The 2.4 GHz band signal can travel a greater distance than other bands. If your smartphone cannot switch Wi-Fi® bands, try moving farther from your router until your phone switches to the 2.4 GHz band. Then, continue setting up the Matter thermostat.

Below is the list of smart home platform* and their supported hub#

Apple Home

Alexa

Google Home

Samsung SmartThings

  • Apple TV 4K (2nd gen)

  • Apple TV 4K (3rd gen, 128 GB)

  • HomePod (2nd gen)

  • HomePod mini

  • Echo (4th gen)

  • Echo Hub

  • Echo Plus (2nd gen)

  • Echo Show 8 (3rd gen)

  • Echo Show 10 (3rd gen)

  • Echo Studio

  • Nest Hub (2nd gen)

  • Nest Hub Max

  • Nest Wi-Fi

  • Nest Wi-Fi Pro

  • SmartThings Hub v3

  • SmartThings Station

*#The list is not comprehensive, make sure to review the specifications of the required smart platform hubs/speakers.

TIP: If you have previously set up a smart home hub (such as Apple Home Kit, Amazon Alexa, or Google Home) and added it to the respective smart home app, make sure that the device has the latest software update installed, and that your phone and app are also up to date for smoother commissioning process.
If the smart home hub is new, make sure that it has the latest software update installed.

Commissioning with Matter

IMPORTANT: Make sure installer setting and user setting are configured before commissioning.

  1. Wake-up the thermostat by pressing any one touch button and then press and hold O button for 2 s to 5 s to enter commissioning mode.

    The thermostat matrix display "Jn" and LED turns yellow to indicate commissioning mode is initiated

  2. Open Matter supported smart home app and scan the Matter code provided with the thermostat.

    TIP: For more information on location of Matter code, Refer Matter setup code.

Wait for few seconds for the thermostat to get commissioned. You can check the progress in the app.
Upon successful commissioning, app show the connected message and LED turns solid yellow.

If any error occurs during commissioning process, thermostat matrix display “Er LED turns red.

Press O touch button to exit and restart Matter Wi-Fi configuration.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.