DUG_Matter Thermostat_ELKO-03

Over the air update

Matter Over The Air (OTA) allows user to receive firmware updates.

To check for a firmware update, go to the device settings in your smart home app. Tap Update to install the latest firmware.
The Matter thermostat will show a loading LED indication while the update is in progress.

Once the update is complete, the thermostat will display the setpoint and the app shows the latest firmware version.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.