DUG_Matter Thermostat_ELKO-01

Installation instruction

Refer to the installation instruction supplied with this product.

See Matter Thermostat 16 A.

NOTE: It is strongly recommended to use a surge protection device in case thermostat is connected in the same circuit with inductive loads (e.g. fluorescent lights, contactors or motor drives).

Insert installation site

  • Recommended installation height: 1 to 1.5 m above the floor.

  • Do not install too close to windows, doors or ventilation openings.

  • Do not install above heaters or other heat sources.

  • Do not cover or install behind curtains.

  • Avoid direct sunlight and light from lamps.

  • Mounting on the cavity wall requires proper sealing of the conduit box or installation tube, to prevent airflow from affecting temperature sensor performance.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?