DUG_Matter Thermostat_ELKO-03

LED indications

Wi-Fi LED indication

Status

Description

No LED

Thermostat is not commissioned to Matter supported app after configuring installer and user setting.

Yellow solid

Disconnected from Wi-Fi.

Blinks white (1 Hz)

Received identify command during pairing.

White solid

Connected to Wi-Fi.

Heating demand LED indication

Status

Description

Blinks white (2 Hz)

Limit sensor error.

Blinks white (0.5 Hz)

Window open detected.

Blinks white (1 Hz)

Floor limit active.

White solid

Heating demand.

No LED

No heating demand.

Matter commissioning

Refer matter commissioning for more information.

Status

User interaction

Description

Matter commissioning

The thermostat matrix display "Jn" and LED turns yellow to indicate joining progress.

Fails to join the network

The thermostat matrix display flashes “Er” and LED turns red when the thermostat fails to join the network.

Showing demand - temperature control modes

Refer setting room temperature for more information.

Status

User interaction

Description

Heating demand

The LED flashes white at 1hz during heating demand.

Installer level 1 / Device preset

Refer installer level 1 for more information.

Status

User interaction

Description

Enter preset selection

By default, thermostat matrix display flashes “P2” if there is no external sensor connected, or “P4” if there is any external sensor connected when the thermostat is first powered on or after a ex-factory reset.

Installer level 2

Refer installer level 2 for more information.

Status

User interaction

Description

Floor probe type

The thermostat matrix display menu number, left most menu depth LED turns white, and LED turns purple.

Min. floor limit

The thermostat matrix display menu number, left most menu depth LED turns white, and LED turns purple.

Max. floor limit

The thermostat matrix display menu number, left most menu depth LED turns white, and LED turns purple.

Control method

The thermostat matrix display menu number, left most menu depth LED turns white, and LED turns purple.

2-pt min On/Off time

The thermostat matrix display menu number, left most menu depth LED turns white, and LED turns purple.

Temporal limit

The thermostat matrix display menu number, left most menu depth LED turns white, and LED turns purple.

Windows open detection

The thermostat matrix display menu number, left most menu depth LED turns white, and LED turns purple.

User settings

Refer User settings for more information

Status

User interaction

Description

Idle brightness

The thermostat matrix display menu number, left most menu depth LED turns white, and LED turns yellow.

Room sensor calibration

The thermostat matrix display menu number, left most menu depth LED turns white, and LED turns yellow.

Floor sensor calibration

The thermostat matrix display menu number, left most menu depth LED turns white, and LED turns yellow.

Minimum setpoint temperature

The thermostat matrix display menu number, left most menu depth LED turns white, and LED turns yellow.

Maximum setpoint temperature

The thermostat matrix display menu number, left most menu depth LED turns white, and LED turns yellow.

Stand-by mode

The thermostat matrix display menu number, left most menu depth LED turns white, and LED turns yellow.

Resetting the device

Refer resetting the device for more information.

Status

User interaction

Description

Reset User Data

The thermostat matrix display 49, left most menu depth LED turns white, and LED turns yellow.

Ex-factory Reset

The thermostat matrix display 99 and LED turns purple.

Temperature display

Status

User interaction

Description

Temperature below minimum display value
OR
Temperature reading error.

Note: The thermostat matrix displays temperature limits -9 °C to 99 °C.

The thermostat matrix display flashes “--” When the temperature is below -9 degrees.

OR

The thermostat matrix display flashes “--” when the thermostat cannot determine the temperature due to an error.

Temperature above maximum display value

Note: The thermostat matrix displays temperature limits -9 °C to 99 °C.

The thermostat matrix display flashes “+ +” when the temperature is above 99 degrees.

Setback schedule

Refer setback schedule for more information.

Status

User interaction

Description

Set hour

The thermostat matrix display h indicating set hour state.

Set minute

The thermostat matrix display m indicating set minute state.

Set day of week

The thermostat matrix display d indicating set day week state.

Setback

The thermostat matrix display Sb indicating set setback scheduled state.

Setback setpoint temperature

The thermostat matrix display T indicating set setpoint temperature state.

Other LED indication

Refer child lock and switching heating mode for more information.

Status

User interaction

Description

Child lock

Child lock enabled

Child lock disabled

The thermostat matrix display lock and unlock status.

Heating mode off

The thermostat matrix display X indicating that heating mode is off.

OTA Update

Over the air (OTA) update is in progress

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.