DUG_Matter Thermostat_ELKO-03

Standalone setback schedule

Setback schedule refers to a schedule programmed directly into a thermostat, independent of any external system or network. This allows the thermostat to operate based on the set schedule without requiring input from other devices or control systems.

IMPORTANT: Connecting the thermostat to the Matter environment will automatically disable the setback schedule.

If the setback schedule is enabled, the thermostat will run the following setback schedule.
NOTE:
  • In the case of a fresh installation or a power-cut with no schedule set or enabled in the thermostat, the thermostat will control to the setpoint.

  • In the event of a power outage or similar situation during a scheduled event (setback schedule enabled), the thermostat maintains the set time and day for 8 hours.

Monday-Friday
Event Time (24 h) Temperature
Morning 06:00-08:00 Setpoint
Daytime 08:00-16:00 Setpoint - 5°C
Evening 16:00-23:00 Setpoint
Night 23:00-06:00 Setpoint - 5°C
Saturday-Sunday
Event Time (24 h) Temperature
Day 08:00-23:00 Setpoint
Night 23:00-08:00 Setpoint - 5°C

When the setback schedule is enabled, if the user changes the setpoint from the thermostat user interface, the entered value will take precedence over the scheduled setpoint until the end of the current time slot.
Example: If the setback schedule is enabled with a setpoint of 19° C, and at 8 am with the current will be setpoint at 14° C (19° C - 5° C), if the user changes the setpoint to 20° C using the + button, this new value will replace the 14° C until the end of the current time slot (4 pm). After that, the setpoint will revert back to 19° C.

To enable and set schedule

  1. Wake-up the thermostat by pressing any one touch button and then press and hold O button for >= 5 s to enter setback schedule.
    Thermostat matrix blinks h indicates that thermostat is in set hour state.

  2. Press +/- button to adjust hour from 0 to 23.

  3. After selecting the hour, press O button for > 1 s to confirm.

    Thermostat saves the hours setting and move to set minutes.
    The thermostat matrix blinks m indicates that thermostat is in set minutes state.

  4. Press +/- button to adjust minutes from 0 to 59.

  5. Press O button for > 1 s to confirm minutes.

    Thermostat saves the minutes setting and move to set day of week.
    The thermostat matrix blinks d indicates that thermostat is in set day of week state.

  6. Press +/- button to change the day from 1 to 7.

    You can specify a schedule to run on any day of the week, from Monday (1) to Sunday (7).

    • 01: Monday

    • 02: Tuesday

    • 03: Wednesday

    • 04: Thursday

    • 05: Friday

    • 06: Saturday

    • 07: Sunday

  7. Press O button for > 1 s to confirm day.

    Thermostat saves the day setting and move to set schedule enable state.
    The thermostat matrix blinks Sb indicating that thermostat is in setback schedule enable state.

  8. Press +/- button to toggle between and .

  9. When thermostat display , press O button for > 1 s to confirm setback selection.

  10. The thermostat matrix blinks T indicating that thermostat is in set setpoint state.
    Press +/- button to set the required setpoint temperature during the scheduled period.

  11. Press O button for > 1 s to confirm setback setpoint.

    IMPORTANT: Make sure to set all parameters before enabling the schedule to avoid error detection.

Setback schedule is enable.

To disable the schedule

  1. Press and hold O button for > 5s to enter setback schedule.

  2. Navigate to setback schedule in the thermostat.

    The thermostat matrix blinks Sb indicating to thermostat is in setback schedule.

  3. Press +/- button to toggle between and .

  4. When thermostat display , press O button for > 1 s to confirm selection.

Setback schedule is disabled.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.