DUG_Matter Thermostat_ELKO-03

Troubleshooting

Symptom

Possible cause

Solution

The thermostat has gone offline.

The thermostat heating mode is Off.

The turn on heating mode. Refer switching heating mode.

Disconnected from Wi-Fi.

Check Wi-Fi connection.

Unable to commission the thermostat with app.

  • Check if the app is Matter compatible.

  • Check network connection.

Thermostat doesn't react to any button pressed

The thermostat is in child lock mode.

Press and hold O and button simultaneously for >10.
Refer child lock.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.