DUG_Matter Thermostat_ELKO-03

Switching on/off the heating mode

When thermostat is not in use, you can turn on/off the device manually.

To turn off heating mode:

NOTE: Make sure to disable child lock before turning off the device.

Wake-up the thermostat by pressing any one touch button and then press touch button for > 5 s to turn off heating mode.

When thermostat heating mode is off:

  • LED displays no room temperature

  • Does not control room temperature

  • Outputs remain off

  • Frost protection will be enabled.

  • On initial interaction, the device shows an “X” on the display to show that it is off.

To turn on heating mode:

Wake-up the thermostat by pressing any one touch button to thermostat matrix display X and then press or O or + button for > 5 s to turn on.

When the thermostat is turned on, it returns to its last state.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.