DUG_Matter Thermostat_ELKO-03

About the device

The ELKO One – Matter Thermostat 16 A (hereinafter referred to as the thermostat) will provide you with a simple, easy to use product to control your heating system and save energy. Covering different heating applications the thermostat is compatible with electric underfloor heating or electric radiators, but it could also be used to control mains-powered motorized valves or circulating pumps for water-based heating.

Thermostat features:

  • Matter-compatible

  • Dot-matrix displays

  • Adjustable brightness for LED

  • Control room temperature setpoint

  • Open window detection

  • Frost Protection

  • Schedule

  • Child lock

Operating elements


Menu level indication

NOTE: All LED indications are explained in the LED behavior chapter.

Matter setup code

You can locate the Matter setup code on both the device and the instruction sheet, which you will need to securely add the product to your smart home network.

IMPORTANT: Keep your Matter setup code in a safe and secure place, and no one else should have a copy of it.
You will need the Matter setup code to add the product to your smart home app.

NOTE: Refer Commissioning with Matter for paring process.

You can find the Matter setup label on the following location.

  1. On the instruction sheet supplied with the product.

  2. On top of the thermostats protective film.

  3. On the back of thermostat logic module.




Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.