DUG_Matter Thermostat_ELKO-03

Setting child lock manually

The child lock feature is designed to prevent children from accessing or inadvertently operating the thermostat. When enabled, users cannot make adjustments to the temperature or other settings on the thermostat..

To enable child lock:

  1. Wake the thermostat by pressing any one touch button.

  2. Press and hold O and button simultaneously for > 5 s.

To disable child lock:

  1. Wake the thermostat by pressing any one touch button.

  2. Press and hold O and button simultaneously for > 10 s.

NOTE: It is still possible to perform a factory reset of the device, even if the child lock feature is enabled. This is to prevent a device from being locked.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.