DUG_Matter Thermostat_ELKO-03

User settings

You can configure LED brightness, sensor calibration, set point limit, and other end user setting.

Based on the preset value set in Installer Level 1, the following parameters can be configured:

Menu

Menu function

System default option

Preset Mode 1

Preset Mode 2

Preset Mode 3

Preset Mode 4

1

Idle brightness

00 (0%)

2

Room sensor calibration

0 (0.0° C)

3

Floor sensor calibration
(If external temperature sensing probe is connected)

0 (0.0° C)

4

Minimum setpoint temperature

For room control (P1 and P2) : 4° C
For floor control (P3 and P4) : 10° C

5

Maximum setpoint temperature

For room control (P1 and P2) : 30 ° C
For floor control (P3 and P4) : 27° C

6

Stand-by mode

(disabled)

: The menu level apply to the preset.
: The menu level does not apply to the preset.

To access user setting menu (menu level 3):

  1. Wake-up the thermostat by pressing any one touch button and then simultaneously press "+" and "" for 5 s. Once you enter user setting, the Wi-Fi LED glows yellow, and left most menu level LED indicator glows white.

  2. Navigate the menu item by pressing "+" or "" touch button and then press “O” touch button for > 1 s to confirm selection.

NOTE: If the thermostat remains inactive for 10 seconds during the process, it will time out and exit the settings.

Idle brightness

You can configure the brightness of the LEDs when thermostat is inactive (after time-out of screen active brightness).

To set idle brightness:

  1. Select menu 1 by pressing O touch button for > 1 s to enter brightness settings.

  2. Press + or touch button on the thermostat to switch between following brightness level.

    • 00: 0% (No display)

    • 01: 10%

    • 02: 25%

    • 03: 50%

    • 04: 75%

    • 05: 100%

  3. Press O touch button for > 1 to confirm selection.

Room sensor calibration

Room sensor calibration involves adjusting and configuring sensors within a room to achieve accurate and reliable measurement of temperature. This process helps in maintaining optimal comfort, energy efficiency, and overall performance of the thermostat.

To set sensor calibration:

  1. Select menu 2 by pressing O touch button for > 1 to enter calibration settings.

  2. Press + or touch button on the thermostat to set the calibration value between.

    NOTE: The temperature calibration ranges from -9° C to +9° C and can be adjusted in 0.5° C increments.
  3. Press O touch button for > 1 to confirm selection.

Floor sensor calibration

Floor sensor calibration involves adjusting and configuring sensors which is connected to floor heating system to achieve accurate and reliable measurement of temperature. This process helps in maintaining optimal comfort, energy efficiency, and overall performance of the thermostat.

To set sensor calibration:

  1. Select menu 3 by pressing O touch button for > 1 to enter calibration settings.

  2. Press + or touch button on the thermostat to set the calibration value between.

    NOTE: The temperature calibration ranges from -9° C to +9° C and can be adjusted in 0.5° C increments.
  3. Press O touch button for > 1 to confirm selection.

Minimum setpoint temperature

You can set the minimum setpoint temperature. It is lower temperature limit you can set in the thermostat.

To set setpoint limit:

  1. Select menu 4 by pressing O touch button for > 1 to enter setpoint settings.

  2. Press + or touch button on the thermostat to set lower temperature limit.

    • Room control ranges from 4° C to 29° C and can be adjusted in 1° C increments.

    • Floor control ranges from 10° C to 39° C and can be adjusted in 1° C increments.
      The minimum floor control setpoint value is determined by the minimum floor limit set in the installer settings.

  3. Press O touch button for > 1 to confirm selection.

NOTE: The minimum setpoint temperature should be lower than maximum setpoint temperature.

Maximum setpoint temperature

You can set the maximum setpoint temperature. It is upper temperature limit you can set in the thermostat.

To set setpoint limit:

  1. Select menu 5 by pressing O touch button for > 1 to enter setpoint settings.

  2. Press + or touch button on the thermostat to set upper temperature limit.

    • Room control ranges from 5° C to 30° C and can be adjusted in 1° C increments.

    • Floor control ranges from 11° C to 40° C and can be adjusted in 1° C increments.
      The maximum floor control setpoint value is determined by the maximum floor limit set in the installer settings.

  3. Press O touch button for > 1 to confirm selection.

NOTE: The maximum setpoint temperature should be higher than minimum setpoint temperature.

Example: When the minimum setpoint limit is set to 12° C and the maximum setpoint limit is set to 28° C, the thermostat allows for a minimum room temperature setting of 12° C and a maximum room temperature setting of 28° C.

Stand-by mode

When room heating is not needed, you can put the thermostat into stand-by mode.

To set stand-by mode:

  1. Select menu 6 by pressing O touch button for > 1 to enter stand-by mode settings.

  2. Press + or touch button on the thermostat to display and then press O touch button for > 1 to confirm selection.

TIP: When thermostat display , press O touch button for > 1 to exit stand-by mode setting.

NOTE: When thermostat is set to stand-by mode:
  • Occupied setpoints is not used.

  • LED display is turned off.

  • Wi-Fi network is turned off.

  • If thermostat is in heating mode, frost protection will be enabled.

To cancel existing stand-by mode, press any touch button for >5 s.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.