DUG_Matter Thermostat_ELKO-03

Installer setting

Thermostat can be configured in two installer levels according to room heating requirement.
IMPORTANT: This process should only be used by authorized/professional installers.
Installer Level 1
Installer Level 1 allows you to set the preset value depending on what the thermostat is directly controlling.
Installer Level 2
Installer Level 2 enables you to configure additional thermostat parameters, enhancing the user's experience in temperature regulation.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.