DUG_Matter Thermostat_ELKO-03

Setting the room temperature

The room temperature can be increased/decreased manually by pressing the touch button on the thermostat.

  • Press the “+” button to increase the temperature setpoint.

  • Press the “” button to decrease the temperature setpoint.

NOTE:
  • Temperature can be adjusted in 0.5°C increments.

  • Max. and Min. temperature setpoint which can be set is based for the limit defined in the user setting.

In P4, if floor sensor is fitted, device will be in room temperature with floor limits mode.

If the room temperature equals or exceeds the setpoint, and the floor temperature is below the lower limit (min. guard), a demand is created, heating the room to warm the floor, and the demand LED flashes white at 1 Hz.

If the room temperature is lower than the setpoint and the floor temperature exceeds the upper limit (max. guard), the demand should be 0, control output should be prevented, and the demand LED flashes white at 1 Hz.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.