DUG_Matter Thermostat_ELKO-03

About the Document

Document Scope

This document provides detailed guidance on the ELKO One Matter Thermostat 16 A, including its features, installation steps, and configuration options. It explains how to set up the thermostat with Matter-compatible smart home systems, adjust presets, and customize installer and user settings for optimal heating control. Users will learn how to manage temperature set points, schedules, child lock, and standby mode, as well as perform resets and firmware updates. The guide also covers LED indications, troubleshooting tips, technical specifications, and compliance details, ensuring a comprehensive understanding of the device’s functionality and integration capabilities.

Validity Note

The characteristics of the products described in this document are intended to match the characteristics that are available on elko.no. As part of our corporate strategy for constant improvement, we may revise the content over time to enhance clarity and accuracy. If you see a difference between the characteristics in this document and the characteristics on elko.no, consider elko.no to contain the latest information.

For your safety

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Safe electrical installation must be carried out only by skilled professionals. Skilled professionals must prove profound knowledge in the following areas:
  • Connecting to installation networks.
  • Connecting several electrical devices.
  • Laying electric cables.
  • Safety standards, local wiring rules and regulations.
Failure to follow these instructions will result in death or serious injury.
DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
The output may carry electric current even when the load is switched off.
  • Disconnect the device from the supply by means of the fuse in the incoming circuit before working on the device.
Failure to follow these instructions will result in death or serious injury.
DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
The device is not a Safety Extra Low Voltage (SELV) device.
The sensor lines are on mains (AC 230 V) line.
  • Only use sensors with double insulated cables.
Failure to follow these instructions will result in death or serious injury.

General Cybersecurity Information

In recent years, the growing number of networked machines and production plants has seen a corresponding increase in the potential for cyber threats, such as unauthorized access, data breaches, and operational disruptions. You must, therefore, consider all possible cybersecurity measures to help protect assets and systems against such threats.

To help keep your Schneider Electric products secure and protected, it is in your best interest to implement the cybersecurity best practices as described in the Cybersecurity Best Practices document.

Schneider Electric provides additional information and assistance:

Cybersecurity

Cybersecurity aims to prevent your system, communication networks, and devices from possible attacks, data tampering, or confidential information leakage.


Following these cybersecurity principles may help to reduce the risk of cyber threats to the network where your system is installed.

  • Keep your phone up-to-date and install the latest security updates.

  • Only connect to secure Wi-Fi networks.

  • Only download apps from Google Play or Apple store.

  • Use all the security settings on your smart phone/tablet:

    • Long passcodes or pass phrases

    • Two-factor authentication (2FA)

    • Facial recognition

    • Block unknown apps

Refer CSA Matter Security Principles.

Secure disposal / End of Life / Decommission

If a device needs to be disposed of, perform a factory reset to delete all data, project data, and programming is deleted from the device. Make sure that it is securely disposed to prevent its redeployment into your operational system or unauthorized use.

Environmental Data

Find and download comprehensive environmental data about your products, including RoHS compliance and REACH declarations as well as Product Environmental Profile (PEP), End-of-Life instructions (EOLI) and much more.


https://www.se.com/myschneider

General information about Schneider Environmental Data Program

Click the link below to read about Schneider Electric’s Environmental Data Program.


https://www.se.com/ww/en/about-us/sustainability/environmental-data-program/

Declaration of Conformity

Hereby, Schneider Electric Industries SAS, declares that this product is in compliance with the essential requirements and other relevant provisions of RADIO EQUIPMENT DIRECTIVE 2014/53/EU.

Declaration of conformity can be downloaded on:

Available Languages of the Document

The document is available in these languages:

  • English

  • Norwegian

Information on Non-Inclusive or Insensitive Terminology

As a responsible, inclusive company, Schneider Electric is constantly updating its communications and products that contain non-inclusive or insensitive terminology. However, despite these efforts, our content may still contain terms that are deemed inappropriate by some customers.

Trademarks

  • Amazon, Alexa and all related logos are trademarks of Amazon.com, Inc. or its affiliates.

  • Apple® and App Store® are brand names or registered trademarks of Apple Inc.

  • Google, Google Home, Google Play Store, and Android are trademarks of Google LLC.

  • Wi-Fi® is a registered trademark of Wi-Fi Alliance®.

Other brands and registered trademarks are the property of their respective owners.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.