990-91379G-022

Perform a Battery SPoT Mode Test in a Single UPS System

OPMERKING: The Battery SPoT mode test is only legally allowed to perform in some countries/areas. Please refer to local/national legislation.

Prerequisites for single UPS system:

  • UOB must be open

  • The UPS operation mode must be Requested static bypass

  • The battery disconnect device(s) BB must be closed

  • There must be no detected surveillance faults

  • SSIB must be closed

  • The output voltage and frequency must be within predefined limits

This feature performs a battery discharge test without the need for a load bank. During the battery SPoT mode test, the inverter is turned ON while the UPS is in requested static bypass. During the test, the UPS performs a battery runtime calibration test (if the battery runtime test prerequisites are met, see Een kalibratietest van de autonomietijd starten) and adjusts the estimated runtime accordingly.

The output power can be manually adjusted from 0 to 100% load to be as close as possible to the operating conditions.

The test stops when the battery voltage has reached its shutdown level, or when the predefined discharge level has been reached.

OPMERKING: Battery SPoT mode must be enabled by Schneider Electric during service configuration before this test is available.
  1. From the home screen on the display, select Tests > Battery SPoT mode.
  2. On page 1 of the menu for Battery SPoT mode, verify that the prerequisites for performing a test is met and confirm that the load is powered if UOB is open during this procedure. Tap the arrow symbol to go to the next page.
  3. On page 2, follow the listed checklist. Tap the arrow symbol to go to the next page.
  4. On page 3, set the battery discharge level and the output power level. Tap the arrow symbol to go to the next page.
  5. On page 4, tap Start battery SPoT mode to start the test.
    OPMERKING: If you wish to manually stop the test, tap Abort battery SPoT mode .
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.