990-91317G-031

Läckström

380/400/415 V UPS-system, installation med 4 ledare vid 100 % last

UPS-storlek Läckström
10-20 kW 60 mA
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.