990–5809D-018

I/Oキャビネットとクラシックバッテリーキャビネット間の信号ケーブルの接続

注記: 以下の図は、4つのバッテリーバンクがそれぞれ1つのクラシックバッテリーキャビネットを構成しているシステムを示しています。設置時にはクラシックバッテリーキャビネットの数に従って信号ケーブルを接続してください。
注記: バッテリーバンク内に2つのクラシックバッテリーキャビネットがある場合、1つのバッテリーバンク内の2つのクラシックバッテリーキャビネット間で信号ケーブルを接続する方法についての詳細は、1つのバッテリーバンク内にある2つのクラシックバッテリーキャビネット間の信号ケーブルの接続を参照してください。
  1. 信号ケーブルをバッテリーバンクからI/Oキャビネットの上部または下部に通して、基板まで配線します。
  2. I/Oキャビネットとクラシックバッテリーキャビネットの間に信号ケーブルを接続します。
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

この情報は役に立ちましたか?