DOCA0105EN-09

Diagnostic Get Commands

List of Commands

The following table lists the diagnostic get commands, their corresponding command codes, and user profiles:

Command

Command code

User profile

Get coil information Get Coil Information

49793

No password required

Get health state Get Health State

49794

No password required

Get trip counters in operation Get Trip Counters in Operation

49795

No password required

Get trip counters in test mode Get Trip Counters in Test Mode

49796

No password required

Get trip counters in manual test mode Get Trip Counters in Manual Test Mode

49797

No password required

Get motor charging operation information Get Motor Charging Operation Information

49798

No password required

Get breaker durability Get Breaker Durability

51328

No password required

Get operating times Get Operating Times

51329

No password required

Get Coil Information

To get the coil information, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

49793

Requested command code

0x1F40

8001

INT16U

11

Number of parameters of the command

0x1F41

8002

INT16U

5377 (0x1501)

Destination of the command

0x1F42

8003

INT16U

0

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

0

Password of the command = 0 (no password required)

0x1F45

8006

INT16U

MSB: Requested coil identification:

  • 16 = MX1 opening voltage release

  • 17 = XF closing voltage release

  • 18 = MN opening undervoltage release

  • 19 = MX2 opening voltage release

LSB: 0 (not used)

The coil information is returned to command registers in the following way:

Address

Register

Unit

Type

Range

Bit

Description

0x1F53

8020

INT16U

49793

Last command code

0x1F54

8021

INT16U

Command status:

0x1F55

8022

INT16U

4

Number of bytes returned

0x1F56

8023

INT16U

1–3

MSB: Responded coil identification:

  • 16 = MX1 opening voltage release

  • 17 = XF closing voltage release

  • 18 = MN opening undervoltage release

  • 19 = MX2 opening voltage release

LSB: 0 (not used)

0x1F58

8024

INT16U

0

Application type:

  • 0 = Opening (MX or MN coil)

  • 1 = Closing (XF coil)

1

Communication status:

  • 0 = Not communicating (standard voltage or undervoltage release)

  • 1 = Communicating

    • MX1 (Diagnostic and communication)

    • XF (Diagnostic and communication)

    • MN or MX2 (Diagnostic)

2

Physical health (release autotest result):

  • 0 = Release malfunction (release needs to be replaced)

  • 1 = Release OK

3

Coil activation status:

  • 0 = Plunger not activated

    • MN diagnostic plunger pull out (opening order activated)

    • MX2 diagnostic plunger pushed in (opening order not activated)

  • 1 = Plunger activated

    • MN diagnostic plunger pushed in (opening order not activated)

    • MX2 diagnostic plunger pull out (opening order activated)

4

Model type:

  • 0 = Not MN undervoltage release

  • 1 = MN undervoltage release

5–7

Reserved

8

Application type quality:

  • 0 = Invalid

  • 1 = Valid

9

Communication status quality:

  • 0 = Invalid

  • 1 = Valid

         

10

Physical health quality:

  • 0 = Invalid

  • 1 = Valid

11

Quality of coil activation status:

  • 0 = Invalid

  • 1 = Valid

12

Model type quality:

  • 0 = Invalid

  • 1 = Valid

13–15

Reserved

Get Health State

To get the health state, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

49794

Requested command code

0x1F40

8001

INT16U

14

Number of parameters of the command

0x1F41

8002

INT16U

5377 (0x1501)

Destination of the command

0x1F42

8003

INT16U

0

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

0

Password of the command = 0 (no password required)

0x1F45–0x1F46

8006–8007

0xFFFFFFFF

Reserved

The health state is returned to command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F53

8020

INT16U

49794

Last command code

0x1F54

8021

INT16U

Command status:

0x1F55

8022

INT16U

6

Number of bytes returned

0x1F56–0x1F57

8023–8024

Reserved

0x1F58

8025

INT16U

MSB: Overall system health state

  • 0 = Not evaluated

  • 1 = Ok

  • 2 = Medium severity alarm detected

  • 3 = High severity alarm detected

LSB: Reserved

Get Trip Counters in Operation

To get the trip counters in operation, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

49795

Requested command code

0x1F40

8001

INT16U

10

Number of parameters of the command

0x1F41

8002

INT16U

5377 (0x1501)

Destination of the command

0x1F42

8003

INT16U

0

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

0

Password of the command = 0 (no password required)

The trip counters in operation is returned to command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F53

8020

INT16U

49795

Last command code

0x1F54

8021

INT16U

Command status:

0x1F55

8022

INT16U

24

Number of bytes returned

0x1F56–0x1F57

8023–8024

INT32U

Number of total trips in operation

0x1F58–0x1F59

8025–8026

INT32U

Number of long time trips in operation

0x1F5A–0x1F5B

8027–8028

INT32U

Number of short time trips in operation

0x1F5C–0x1F5D

8029–8030

INT32U

Number of instantaneous trips in operation

0x1F5E–0x1F5F

8031–8032

INT32U

Number of ground/earth leakage fault trips in operation

0x1F60–0x1F61

8033–8034

INT32U

Number of other trips in operation

Get Trip Counters in Test Mode

To get the trip counters in test mode, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

49796

Requested command code

0x1F40

8001

INT16U

10

Number of parameters of the command

0x1F41

8002

INT16U

5377 (0x1501)

Destination of the command

0x1F42

8003

INT16U

0

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

0

Password of the command = 0 (no password required)

The trip counters in test mode is returned to command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F53

8020

INT16U

49796

Last command code

0x1F54

8021

INT16U

Command status:

0x1F55

8022

INT16U

12

Number of bytes returned

0x1F56–0x1F57

8023–8024

INT32U

Number of total trips in test mode

0x1F58–0x1F5B

8025–8028

DATETIME

Date/Time of last trip in test mode

Get Trip Counters in Manual Test Mode

To get the trip counters in manual test mode, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

49797

Requested command code

0x1F40

8001

INT16U

10

Number of parameters of the command

0x1F41

8002

INT16U

5377 (0x1501)

Destination of the command

0x1F42

8003

INT16U

0

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

0

Password of the command = 0 (no password required)

The trip counters in manual test mode is returned to command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F53

8020

INT16U

49797

Last command code

0x1F54

8021

INT16U

Command status:

0x1F55

8022

INT16U

12

Number of bytes returned

0x1F56–0x1F57

8023–8024

INT32U

Number of total trips in manual test mode

0x1F58–0x1F5B

8025–8028

DATETIME

Date/Time of last trip in manual test mode

Get Motor Charging Operation Information

To get the motor charging operation information, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

49798

Requested command code

0x1F40

8001

INT16U

10

Number of parameters of the command

0x1F41

8002

INT16U

5377 (0x1501)

Destination of the command

0x1F42

8003

INT16U

0

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

0

Password of the command = 0 (no password required)

The motor charging operation information is returned to command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F53

8020

INT16U

49798

Last command code

0x1F54

8021

INT16U

Command status:

0x1F55

8022

INT16U

8

Number of bytes returned

0x1F56–0x1F57

8023–8024

INT32U

Motor charging operation counter

0x1F58–0x1F59

8025–8026

s

FLOAT32

Motor last charging time after closing

Get Breaker Durability

To get the breaker durability information, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

51328

Requested command code

0x1F40

8001

INT16U

10

Number of parameters of the command

0x1F41

8002

INT16U

5377 (0x1501)

Destination of the command

0x1F42

8003

INT16U

0

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

0

Password of the command = 0 (no password required)

The breaker durability information is returned to command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F53

8020

INT16U

51328

Last command code

0x1F54

8021

INT16U

Command status:

0x1F55

8022

INT16U

28

Number of bytes returned

0x1F56–0x1F57

8023–8024

INT32U

Total number of operations (opening operation counter)

0x1F58–0x1F59

8025–8026

INT32U

Number of operation with load › 0.4 In

0x1F5A–0x1F5B

8027–8028

FLOAT32

0-1

Breaker remaining service life ratio:

  • 0 = End of typical service life of the breaker

  • 1 = Breaker is new

0x1F5C–0x1F63

8029–8036

Reserved

Get Operating Times

To get the operating time information, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

51329

Requested command code

0x1F40

8001

INT16U

10

Number of parameters of the command

0x1F41

8002

INT16U

5377 (0x1501)

Destination of the command

0x1F42

8003

INT16U

0

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

0

Password of the command = 0 (no password required)

The operating time information is returned to command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F53

8020

INT16U

51329

Last command code

0x1F54

8021

INT16U

Command status:

0x1F55

8022

INT16U

8

Number of bytes returned

0x1F56–0x1F57

8023–8024

s

INT32U

Time of use

0x1F58–0x1F59

8025–8026

s

INT32U

Operating time with load

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.