DOCA0105EN-09

Peak Values of Demand Values of Real-Time Measurements

Current Peak Demand Values

Current peak demand values can be reset with the reset minimum/maximum command.

Address

Register

RW

Unit

Type

Range

Description

0x7DA9–0x7DAA

32170–32171

R

A

FLOAT32

Current peak demand value on phase 1: I1 dmd max

0x7DAB–0x7DAC

32172–32173

R

A

FLOAT32

Current peak demand value on phase 2: I2 dmd max

0x7DAD–0x7DAE

32174–32175

R

A

FLOAT32

Current peak demand value on phase 3: I3 dmd max

0x7DAF–0x7DB0

32176–32177

R

A

FLOAT32

Current peak demand value on the neutral: IN dmd max(1)

0x7DF3–0x7DF4

32244–32245

R

A

FLOAT32

Average peak current demand

(1) Value available when system type register returns 30 or 41.

Power Peak Demand Values

Power peak demand values can be reset with the reset minimum/maximum command.

Address

Register

RW

Unit

Type

Range

Description

0x7DB1–0x7DB2

32178–32179

R

W

FLOAT32

Total active power peak demand: P dmd max

0x7DB3–0x7DB4

32180–32181

R

VAR

FLOAT32

Total reactive power peak demand: Q dmd max

0x7DB5–0x7DB6

32182–32183

R

VA

FLOAT32

Total apparent power peak demand: S dmd max

Timestamp of Peak Demand Values and Reset of Peak Demand Values

Address

Register

RW

Unit

Type

Range

Description

0x8940–0x8943

35137–35140

R

DATETIME

Timestamp of peak current demand on neutral

0x8944–0x8947

35141–35144

R

DATETIME

Timestamp of average peak current demand

0x8948–0x894B

35145–35148

R

DATETIME

Timestamp of last reset of peak demand current

0x894C–0x894F

35149–35152

R

DATETIME

Timestamp of last reset of peak demand power

0x8950–0x8953

35153–35156

R

DATETIME

Timestamp of peak demand current on phase 1

0x8954–0x8957

35157–35160

R

DATETIME

Timestamp of peak demand current on phase 2

0x8958–0x895B

35161–35164

R

DATETIME

Timestamp of peak demand current on phase 3

0x895C–0x895F

35165–35168

R

DATETIME

Timestamp of peak demand active power

0x8960–0x8963

35169–35172

R

DATETIME

Timestamp of peak demand reactive power

0x8964–0x8967

35173–35176

R

DATETIME

Timestamp of peak demand apparent power

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.