DOCA0105EN-09

Circuit Breaker Operation Set Commands

List of Commands

The following table lists the circuit breaker operation set commands, their corresponding command codes, and user profiles:

Command

Command code

User profile

Open circuit breaker Open Circuit Breaker

904

Administrator or Operator

Close circuit breaker Close Circuit Breaker

905

Administrator or Operator

Set close breaker inhibition Set Close Breaker Inhibition

910

Administrator or Operator

Open Circuit Breaker

To open the circuit breaker, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

904

Requested command code

0x1F40

8001

INT16U

10

Number of parameters of the command

0x1F41

8002

INT16U

5377 (0x1501)

Destination of the command

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

Password of the command: Administrator or Operator user profile password

NOTE: After use of the open circuit breaker command, check that the circuit breaker is open in register 32001.

Close Circuit Breaker

To close the circuit breaker, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

905

Requested command code

0x1F40

8001

INT16U

10

Number of parameters of the command

0x1F41

8002

INT16U

5377 (0x1501)

Destination of the command

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

Password of the command: Administrator or Operator user profile password

NOTE: After use of the close circuit breaker command, check that the circuit breaker is closed in register 32001.

Set Close Breaker Inhibition

To enable or inhibit the close circuit breaker command, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

910

Requested command code

0x1F40

8001

INT16U

13

Number of parameters of the command

0x1F41

8002

INT16U

5377 (0x1501)

Destination of the command

0x1F42

8003

INT16U

1

Security type of the command

0x1F43-0x1F44

8004–8005

OCTET STRING

Password of the command: Administrator or Operator user profile password

0x1F45

8006

INT16U

0–1

Close breaker inhibited by communication:

  • 0 = Enable close order

  • 1 = Inhibit close order

0x1F46

8007

INT16U

1

Origin of the command:

  • 1 = close breaker enable/inhibit command from remote controller using the communication network

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.