DOCA0105EN-09

List of MicroLogic Control Unit Protection Commands with Session and Error Codes

List of Commands

The MicroLogic control unit protection commands with session are performed by the command interface. They are grouped by their functions and types:

In the MicroLogic control unit registers:

  • RC indicates the registers that can be read by a get command

  • WC indicates the registers that can be written by a set and reset command

Error Codes

Error codes generated by MicroLogic control units are the generic error codes Result of the Command.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.