DOCA0105EN-09

Measurement Settings Set Commands

List of Commands

The following table lists the measurement settings set commands, their corresponding command codes, and user profiles:

Command

Command code

User profile

Set power flow sign configuration Set Power Flow Sign Configuration

47240

Administrator

Set power factor sign convention Set Power Factor Sign Convention

47241

Administrator

Set energy accumulation mode Set Energy Accumulation Mode

47242

Administrator

Set current demand configuration Set Current Demand Configuration

47243

Administrator

Set power demand configuration Set Power Demand Configuration

47244

Administrator

Set Power Flow Sign Configuration

To set the power flow sign configuration, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

47240

Requested command code

0x1F40

8001

INT16U

12

Number of parameters of the command

0x1F41

8002

INT16U

5377 (0x1501)

Destination of the command

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

Password of the command: Administrator user profile password

0x1F45

8006

INT16U

0–1

Power sign

  • 0 = Direct or P+ = the active power flows from upstream (top) to downstream (bottom) (factory setting)

  • 1 = Inverted or P– = the active power flows from downstream (bottom) to upstream (top)

Set Power Factor Sign Convention

To set the power factor sign convention, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

47241

Requested command code

0x1F40

8001

INT16U

12

Number of parameters of the command

0x1F41

8002

INT16U

5377 (0x1501)

Destination of the command

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

Password of the command: Administrator user profile password

0x1F45

8006

INT16U

0, 2

Power factor sign convention:

  • 0 = IEC

  • 2 = IEEE (factory setting)

Set Energy Accumulation Mode

To set the energy accumulation mode, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

47242

Requested command code

0x1F40

8001

INT16U

12

Number of parameters of the command

0x1F41

8002

INT16U

5377 (0x1501)

Destination of the command

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

Password of the command: Administrator user profile password

0x1F45

8006

INT16U

0–1

Energy accumulation mode:

  • 0 = Absolute (factory setting)

  • 1 = Signed

Set Current Demand Configuration

To set the current demand configuration, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

47243

Requested command code

0x1F40

8001

INT16U

12

Number of parameters of the command

0x1F41

8002

INT16U

5377 (0x1501)

Destination of the command

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

Password of the command: Administrator user profile password

0x1F45

8006

min

INT16U

1–60

Current demand calculation interval time

Set Power Demand Configuration

To set the power demand configuration, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

47244

Requested command code

0x1F40

8001

INT16U

14

Number of parameters of the command

0x1F41

8002

INT16U

5377 (0x1501)

Destination of the command

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

Password of the command: Administrator user profile password

0x1F45

8006

INT16U

0

Power demand calculation method:

  • 0 = sliding window

0x1F46

8007

min

INT16U

1-60

Power demand calculation interval time

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.