DOCA0105EN-09

Legacy Dataset

Description

The legacy dataset contains the most useful information of each IMU module in one convenient table. The legacy dataset is available in the registers 12000 to12165. It can be read with two read requests.

Each IMU module updates the values in the dataset registers on a regular basis.

The response time of requests to legacy dataset registers is shorter than the response time of requests to device registers. Therefore, it is recommended to read the legacy dataset registers instead of device registers, to improve the overall performance of the system Modbus Programming Recommendations.

NOTE:
  • The legacy dataset is compatible with legacy versions of the MicroLogic trip unit for ComPacT NSX, PowerPacT H-,J-, and L-frame, ComPacT NS, PowerPacT P-, and R-frame or MasterPact NT/NW circuit breaker. For this reason, data read directly in the Modbus registers is organized in a different way than in the standard dataset.

  • For new applications, it is recommended to use the standard dataset instead of the legacy dataset.

Data Availability

The legacy dataset is available when the Modbus legacy dataset Digital Module is purchased and installed on a MicroLogic X control unit.

The Modbus legacy dataset Digital Module is compatible with MicroLogic X control units with firmware version greater than or equal to version V002.000.xxx.

The Modbus legacy dataset is available on a remote controller using the communication network through the following communication interfaces:

  • IFE Ethernet interface

  • EIFE Ethernet interface

  • IFE server

  • IFM Modbus-SL interface

The following table shows the part numbers and firmware versions necessary to access the Modbus legacy dataset through communication interfaces:

Communication interface

Part number

Minimum firmware version required

IFE Ethernet interface

LV434010

V003.007.024

LV434001

IFE server

LV434011

V003.007.024

LV434002

EIFE Ethernet interface

LV851001

V003.007.024

IFM Modbus-SL interface

LV434000

V003.001.006

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?