Application Commands
Preset Cradle/Drawer Counters
The cradle/drawer counter values can be read from the cradle management registers.
To preset the cradle or drawer counters, set the command registers in the following way:
|
Address |
Register |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
INT16U |
41352 |
Command code = 41352 |
|
0x1F40 |
8001 |
– |
INT16U |
16 |
Number of parameters (bytes) = 16 |
|
0x1F41 |
8002 |
– |
INT16U |
– |
Destination =
|
|
0x1F42 |
8003 |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43–0x1F44 |
8004– 8005 |
– |
OCTET STRING |
– |
Password of the command: Administrator or Operator user profile password |
|
0x1F45 |
8006 |
– |
INT16U |
0–65535 |
Connected counter reset/preset:
|
|
0x1F46 |
8007 |
– |
INT16U |
0–65535 |
Disconnected counter reset/preset:
|
|
0x1F47 |
8008 |
– |
INT16U |
0–65535 |
Test counter reset/preset:
|
Preset Regrease Timers
To preset regrease timers, set the command registers in the following way:
|
Address |
Register |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
INT16U |
41353 |
Command code = 41353 |
|
0x1F40 |
8001 |
– |
INT16U |
18 |
Number of parameters (bytes) = 18 |
|
0x1F41 |
8002 |
– |
INT16U |
– |
Destination =
|
|
0x1F42 |
8003 |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43–0x1F44 |
8004– 8005 |
– |
OCTET STRING |
– |
Password of the command: Administrator or Operator user profile password |
|
0x1F45–0x1F46 |
8006–8007 |
– |
INT16U |
– |
Operating time since last grease maintenance
|
|
0x1F47–0x1F48 |
8008–8009 |
INT32U |
– |
Operating time since last move in rack in position (delay from last disconnection)
|
Light Control
The light command status can be read from the light control registers.
To control the light, set the command registers in the following way:
|
Address |
Register |
Unit |
Type |
Range |
Bit |
Description |
|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
INT16U |
42120 |
– |
Command code = 42120 |
|
0x1F40 |
8001 |
– |
INT16U |
13 |
– |
Number of parameters (bytes) = 13 |
|
0x1F41 |
8002 |
– |
INT16U |
– |
– |
Destination = IO 1: 8193 (0x2001) |
|
0x1F42 |
8003 |
– |
INT16U |
1 |
– |
Security type of the command |
|
0x1F43–0x1F44 |
8004– 8005 |
– |
OCTET STRING |
– |
– |
Password of the command: Administrator or Operator user profile password |
|
0x1F45 |
8006 |
– |
INT16U |
– |
– |
MSB: State |
|
0 |
|
|||||
|
1 |
|
|||||
|
– |
LSB = Timer (MSB) 1–54000 seconds (if bit 1 in set state) Any value 0-0xffff (if bit 1 in reset state) |
|||||
|
0x1F46 |
8007 |
– |
INT16U |
– |
– |
MSB = Timer (LSB) 1 to 54000 seconds (if bit 1 is in set state) Any value 0-0xffff (if bit 1 is in reset state) LSB = 0 (not used) |
Load Control
The load command status can be read from the load control registers.
To control the load, set the command registers in the following way:
|
Address |
Register |
Unit |
Type |
Range |
Bit |
Description |
|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
INT16U |
42376 |
– |
Command code = 42376 |
|
0x1F40 |
8001 |
– |
INT16U |
13 |
– |
Number of parameters (bytes) = 13 |
|
0x1F41 |
8002 |
– |
INT16U |
– |
– |
Destination = IO 1: 8193 (0x2001) |
|
0x1F42 |
8003 |
– |
INT16U |
1 |
– |
Security type of the command |
|
0x1F43–0x1F44 |
8004– 8005 |
– |
OCTET STRING |
– |
– |
Password of the command: Administrator or Operator user profile password |
|
0x1F45 |
8006 |
– |
INT16U |
– |
– |
MSB: State |
|
0 |
|
|||||
|
1 |
|
|||||
|
– |
LSB = Timer (MSB) 1–54000 seconds (if bit 1 in set state) Any value 0-0xffff (if bit 1 in reset state) |
|||||
|
0x1F46 |
8007 |
– |
INT16U |
– |
– |
MSB = Timer (LSB) 1–54000 seconds (if bit 1 in set state) Any value 0-0xffff (if bit 1 in reset state) |
|
– |
LSB = 0 (not used) |
Preset Input Pulse Counters
To preset pulse counters, set the command registers in the following way:
|
Address |
Register |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
INT16U |
42888 |
Command code = 42888 |
|
0x1F40 |
8001 |
– |
INT16U |
34 |
Number of parameters (bytes) = 34 NOTE: The number of parameters corresponds to the
number of bytes of the 17 registers 8001–8015 and 8022–8023.
The bytes of the registers 8016–8021 are not counted as command
parameters.
|
|
0x1F41 |
8002 |
– |
INT16U |
– |
Destination =
|
|
0x1F42 |
8003 |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43–0x1F44 |
8004– 8005 |
– |
OCTET STRING |
– |
Password of the command: Administrator or Operator user profile password |
|
0x1F45–0x1F46 |
8006– 8007 |
– |
INT32U |
0–4294967295 |
I1 pulse counter reset/preset:
|
|
0x1F47–0x1F48 |
8008– 8009 |
– |
INT32U |
0–4294967295 |
I2 pulse counter reset/preset:
|
|
0x1F49–0x1F4A |
8010– 8011 |
– |
INT32U |
0–4294967295 |
I3 pulse counter reset/preset:
|
|
0x1F4B–0x1F4C |
8012– 8013 |
– |
INT32U |
0–4294967295 |
I4 pulse counter reset/preset:
|
|
0x1F4D–0x1F4E |
8014– 8015 |
– |
INT32U |
0–4294967295 |
I5 pulse counter reset/preset:
|
|
0x1F4F |
8016 |
– |
– |
– |
Must be set to 0 (factory setting). |
|
0x1F50 |
8017 |
– |
– |
– |
Must be set to 8019 (factory setting). |
|
0x1F51 |
8018 |
– |
– |
– |
Must be set to 8020 (factory setting). |
|
0x1F52 |
8019 |
– |
– |
– |
Must be set to 8021 (factory setting). |
|
0x1F53 |
8020 |
– |
– |
– |
Must be set to 0. |
|
0x1F54 |
8021 |
– |
– |
– |
Must be set to 0. |
|
0x1F55–0x1F56 |
8022– 8023 |
– |
INT32U |
0–4294967295 |
I6 pulse counter reset/preset:
|
Preset Switchboard Temperature Threshold Counters
To preset switchboard temperature threshold counters, set the command registers in the following way:
|
Address |
Register |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
INT16U |
42889 |
Command code = 42889 |
|
0x1F40 |
8001 |
– |
INT16U |
16 |
Number of parameters (bytes) = 16 |
|
0x1F41 |
8002 |
– |
INT16U |
– |
Destination =
|
|
0x1F42 |
8003 |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43–0x1F44 |
8004– 8005 |
– |
OCTET STRING |
– |
Password of the command: Administrator or Operator user profile password |
|
0x1F45 |
8006 |
– |
INT16U |
0–65535 |
Switchboard temperature threshold 1 counter reset/preset:
|
|
0x1F46 |
8007 |
– |
INT16U |
0–65535 |
Switchboard temperature threshold 2 counter reset/preset:
|
|
0x1F47 |
8008 |
– |
INT16U |
0–65535 |
Switchboard temperature threshold 3 counter reset/preset:
|