Alarm Status
Addresses and Registers List
The following table describes the alarm status addresses, and registers regarding the IO module.
|
IO Module |
Addresses |
Registers |
|---|---|---|
|
IO 1 |
0x3989–0x39A6 |
14730–14759 |
|
IO 2 |
0x4541–0x455E |
17730–17759 |
Generic Alarm Status for IO 1
The order and the description of the generic alarm status registers for IO 2 are the same as those of IO 1.
|
Address |
Register |
RW |
Unit |
Type |
Range |
Bit |
Description |
|---|---|---|---|---|---|---|---|
|
0x3989 |
14730 |
R |
– |
INT16U |
– |
– |
Quality of each bit of register 14731:
|
|
0x398A |
14731 |
R |
– |
INT16U |
– |
– |
IO module history format register |
|
0 |
ULP format |
||||||
|
1 |
TI086 format |
||||||
|
2–15 |
Reserved |
||||||
|
0x398B |
14732 |
R |
– |
INT16U |
– |
– |
Quality of each bit of register 14733:
|
|
0x398C |
14733 |
R |
– |
INT16U |
– |
– |
IO module command type Factory setting = 3, both write command mechanisms are enabled. |
|
0 |
1 = Complex commands |
||||||
|
1 |
1 = Simple commands Simple commands can be disabled by sending a command |
||||||
|
2–15 |
Reserved |
||||||
|
0x398D–0x3992 |
14734–14739 |
– |
– |
– |
– |
– |
Reserved |
|
0x3993 |
14740 |
R |
– |
INT16U |
– |
– |
Quality of each bit of register 14741:
|
|
0x3994 |
14741 |
R |
– |
INT16U |
– |
– |
IO module generic alarm 1 status register. |
|
0 |
IO module in STOP mode: IO module is not working and must be replaced. |
||||||
|
1 |
IO module in ERROR mode: IO module is working in degraded mode. |
||||||
|
2 |
Threshold overrun on I1 counter |
||||||
|
3 |
Threshold overrun on I2 counter |
||||||
|
4 |
Threshold overrun on I3 counter |
||||||
|
5 |
Threshold overrun on I4 counter |
||||||
|
6 |
Threshold overrun on I5 counter |
||||||
|
7 |
Threshold overrun on I6 counter |
||||||
|
8 |
Threshold overrun on O1 counter |
||||||
|
9 |
Threshold overrun on O2 counter |
||||||
|
10 |
Threshold overrun on O3 counter |
||||||
|
11 |
Switchboard temperature threshold 1 overrun |
||||||
|
12 |
Switchboard temperature threshold 2 overrun |
||||||
|
13 |
Switchboard temperature threshold 3 overrun |
||||||
|
14–15 |
Reserved |
||||||
|
0x3995 |
14742 |
R |
– |
INT16U |
– |
– |
Quality of each bit of register 14743:
|
|
0x3996 |
14743 |
R |
– |
INT16U |
– |
– |
IO module generic alarm 2 status register. |
|
0 |
User-defined input 1 alarm |
||||||
|
1 |
User-defined input 2 alarm |
||||||
|
2 |
User-defined input 3 alarm |
||||||
|
3 |
User-defined input 4 alarm |
||||||
|
4 |
User-defined input 5 alarm |
||||||
|
5 |
User-defined input 6 alarm |
||||||
|
6–15 |
Reserved |
Cradle and Drawer Management Alarms for IO 1
|
Address |
Register |
RW |
Unit |
Type |
Range |
Bit |
Description |
|---|---|---|---|---|---|---|---|
|
0x3997 |
14744 |
R |
– |
INT16U |
– |
– |
Quality of each bit of register 14745:
|
|
0x3998 |
14745 |
R |
– |
INT16U |
– |
– |
Cradle management alarms register |
|
0 |
Cradle position discrepancy |
||||||
|
1 |
Disconnection of the circuit breaker from cradle is overdue. |
||||||
|
2 |
Cradle has reached its maximum number of operation |
||||||
|
3 |
Remaining service life of cradle is below alarm threshold |
||||||
|
4 |
New MicroLogic control unit has been detected |
||||||
|
5–7 |
Reserved |
||||||
|
8 |
Drawer position discrepancy |
||||||
|
9–15 |
Reserved |
Motor Alarms for IO 1
|
Address |
Register |
RW |
Unit |
Type |
Range |
Bit |
Description |
|---|---|---|---|---|---|---|---|
|
0x3999 |
14746 |
R |
– |
INT16U |
– |
– |
Quality of each bit of register 14747:
|
|
0x399A |
14747 |
R |
– |
INT16U |
– |
– |
IO motor alarms |
|
0–15 |
Reserved |
Miscellaneous Application Alarms for IO 1
|
Address |
Register |
RW |
Unit |
Type |
Range |
Bit |
Description |
|---|---|---|---|---|---|---|---|
|
0x399B |
14748 |
R |
– |
INT16U |
– |
– |
Quality of each bit of register 14749:
|
|
0x399C |
14749 |
R |
– |
INT16U |
– |
– |
Other application alarms register |
|
0 |
Auxiliary contact of load contactor 1 is not closed. |
||||||
|
1 |
Auxiliary contact of load contactor 1 is not opened. |
||||||
|
2 |
Reserved |
||||||
|
3 |
Dual settings 2-wire input discrepancy |
||||||
|
4–15 |
Reserved |
||||||
|
0x399D |
14750 |
R |
– |
INT16U |
– |
– |
Quality of each bit of register 14751:
|
|
0x399E |
14751 |
R |
– |
INT16U |
– |
– |
Predefined input alarms register |
|
0 |
Earth-leakage trip signal contact (SDV) |
||||||
|
1 |
Control voltage presence contact |
||||||
|
2 |
Surge protection status contact |
||||||
|
3 |
Surge failure contact |
||||||
|
4 |
Switch-disconnector ON/OFF indication contact (OF) |
||||||
|
5 |
Fuse blown indication contact |
||||||
|
6 |
Emergency stop |
||||||
|
7 |
Switchboard temperature contact |
||||||
|
8 |
Switchboard ventilation contact |
||||||
|
9 |
Switchboard door contact |
||||||
|
10–15 |
Reserved |
||||||
|
0x399F |
14752 |
R |
– |
INT16U |
– |
– |
Quality of each bit of register 14753:
|
|
0x39A0 |
14753 |
R |
– |
INT16U |
– |
– |
IO module discrepancy alarms register |
|
0 |
Critical hardware discrepancy |
||||||
|
1 |
Critical firmware discrepancy |
||||||
|
2 |
Non-critical hardware discrepancy |
||||||
|
3 |
Non-critical firmware discrepancy |
||||||
|
4–15 |
Reserved |
||||||
|
0x39A1–0x39A6 |
14754–14759 |
– |
– |
– |
– |
– |
Reserved |
@ Justine > Define and rename ULP and TI086 formats of the IO module event history