DOCA0105EN-09

Demand Values of Real-Time Measurements

Current Demand Values

Address

Register

RW

Unit

Type

Range

Description

0x7D9B–0x7D9C

32156–32157

R

A

FLOAT32

Current demand value on phase 1: I1 Dmd

0x7D9D–0x7D9E

32158–32159

R

A

FLOAT32

Current demand value on phase 2: I2 Dmd

0x7D9F–0x7DA0

32160–32161

R

A

FLOAT32

Current demand value on phase 3: I3 Dmd

0x7DA1–0x7DA2

32162–32163

R

A

FLOAT32

Current demand value on the neutral: IN Dmd(1)

(1) Value available when system type register returns 30 or 41.

Power Demand Values

Address

Register

RW

Unit

Type

Range

Description

0x7DA3–0x7DA4

32164–32165

R

W

FLOAT32

Total active power demand: P Dmd

0x7DA5–0x7DA6

32166–32167

R

VAR

FLOAT32

Total reactive power demand: Q Dmd

0x7DA7–0x7DA8

32168–32169

R

VA

FLOAT32

Total apparent power demand: S Dmd

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.