DOCA0105EN-09

Schematics with MasterPact MTZ Circuit Breakers

Description

The IFM interface is connected to the MasterPact MTZ circuit breaker through its ULP port module.

For more information, refer to DOCA0093EN ULP (Universal Logic Plug) System for ComPact and MasterPact Circuit Breakers – User Guide.

ULP Connection

NOTICE
HAZARD OF EQUIPMENT DAMAGE
Failure to follow these instructions can result in equipment damage.

All the connection configurations require the RJ45 ULP cord.

When the second RJ45 ULP port is not used, it must be closed with an ULP line termination.

A

RJ45 ULP cord

B

ULP line termination

Connection of the IFM Interface to a MasterPact MTZ Circuit Breaker

Connect the IFM interface to the ULP port module on a MasterPact MTZ circuit breaker by using the ULP cord.

A

IFM Modbus-SL interface for one circuit breaker

B

ULP line termination

C

RJ45 ULP cord

D

ULP port module

E

MasterPact MTZ fixed circuit breaker

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.