Hardware Setting
Addresses and Registers List
The following table describes the hardware settings addresses, and registers regarding the IO module.
|
IO Module |
Addresses |
Registers |
|---|---|---|
|
IO 1 |
0x38FD–0x3902 |
14590–14595 |
|
IO 2 |
0x44B5–0x44BA |
17590–17595 |
Hardware Setting Registers for IO 1
The order and the description of the hardware setting registers for IO 2 are the same as those of IO 1.
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x38FD |
14590 |
R |
– |
INT16U |
1–9 |
Application rotary switch current position:
|
|
0x38FE |
14591 |
R |
– |
INT16U |
0–1 |
Remote setup padlock position:
|
|
0x38FF |
14592 |
R |
– |
INT16U |
0–1 |
Dip switch1 position:
|
|
0x3900 |
14593 |
– |
– |
– |
– |
Reserved |
|
0x3901 |
14594 |
R |
– |
INT16U |
1–9 |
Last validated application set by the test button located on the front of the IO module:
|
|
0x3902 |
14595 |
R |
– |
INT16U |
1–9 |
Last validated application set by the EcoStruxure Power Commission software:
|
|
0x3903–0x3904 |
14596– 14597 |
– |
– |
– |
– |
Reserved |