DOCA0105EN-09

IFE/EIFE Interface Identification and Status Registers

IFE/EIFE Interface Firmware Revision

The IFE/EIFE interface firmware revision starts at register 11776 and has a maximum length of eight registers.

The firmware revision is an ASCII string using the format XXX.YYY.ZZZ with:

  • XXX = major version (000–127)

  • YYY = minor version (000–255)

  • ZZZ = revision number (000–255)

The NULL character ends the revision number.

Address

Register

RW

Unit

Type

Range

Description

0x2DDF–0x2DEE

11744–11759

R

OCTET STRING

Device family

0x2DEF–0x2DF6

11760–11767

R

OCTET STRING

Product range

0x2DF7–0x2DFE

11768–11775

R

OCTET STRING

Product model

0x2DFF–0x2E04

11776–11781

R

OCTET STRING

Firmware revision

IFE/EIFE Interface Hardware Revision

The IFE/EIFE interface hardware revision starts at register 11784 and has a maximum length of eight registers.

The hardware revision is an ASCII string using the format XXX.YYY.ZZZ with:

  • XXX = major version (000127)

  • YYY = minor version (000255)

  • ZZZ = revision number (000255)

The NULL character ends the revision number.

Address

Register

RW

Unit

Type

Range

Description

0x2E07–0x2E0C

11784–11789

R

OCTET STRING

Hardware revision

IMU Identification

Identification of the IMU can be set by using the EcoStruxure Power Commission software. When not programmed, the IMU identification registers return 0 (0x0000).

The FDM121 display displays the first 14 characters of the IMU name.

Address

Register

RW

Unit

Type

Range

Description

0x2801–0x2820

10242–10273

R-WC

OCTET STRING

User application name

Device name used for acquiring the IP address using DHCP and also the friendly name on DPWS device discovery.

Example: IFE-0A129F’

Maximum length is 64 characters.

Address

Register

RW

Unit

Type

Range

Description

0x2E2F–0x2E38

11824–11833

R

OCTET STRING

Vendor name = ‘Schneider Electric’

0x2E39–0x2E42

11834–11843

R

OCTET STRING

Product code:

  • 'LV434001' or 'LV434010' = IFE-Ethernet com Modbus TCP/IP

  • 'LV434002' or 'LV434011' = IFE-Ethernet com Modbus TCP/IP master

  • ’LV851001’ = EIFE Embedded Ethernet interface

0x2E43–0x2E44

11844–11845

Reserved

Locking Pad Position

Address

Register

RW

Unit

Type

Range

Description

0x2E72

11891

R

INT16U

1,3

Locking pad position

  • 1 = locking pad is in the locked position

  • 3 = locking pad is in the unlocked position

Current Date and Time

Address

Register

RW

Unit

Type

Range

Description

0x2E73–0x2E76

11892–11895

R-WC

DATETIME

Current date and time in DATETIME format

0x2E77–

0x2E78

11896–

11897

R

Seconds

INT32U

0x00–0xFFFFFFFF

Number of seconds counted since last start

Product Identification

Address

Register

RW

Unit

Type

Range

Description

0x2E7C

11901

R

INT16U

17100–17101

Product identification:

  • 17100 for IFE Ethernet interface for one circuit breaker (‘LV434001’ or ‘LV434010’)

  • 17101 for IFE Ethernet switchboard server (‘LV434002’ or ‘LV434011’)

  • 17107 for EIFE embedded Ethernet interface (‘LV851001’)

Validity Duration of Data

Address

Register

RW

Unit

Type

Range

Description

0x306A

12395

R

s

INT16U

5–300 (in step of 5 s)

Duration of validity of data in the dataset

Read Device Identification

The Read Device Identification function is used to access in a standardized manner the information required to identify a device clearly. The description is made up of a set of objects (ASCII character strings).

A complete description of the Read Device Identification function is available at www.modbus.org.

The coding for the identification of the IFE/EIFE interface is the following:

Name

Type

Description

Vendor name

OCTET STRING

‘Schneider Electric’ (18 characters)

Product code

OCTET STRING

  • 'LV434001' or 'LV434010'

  • 'LV434002' or 'LV434011'

  • ‘LV851001’ (EIFE)

Firmware revision

OCTET STRING

‘XXX.YYY.ZZZ’

Vendor URL

OCTET STRING

‘www.se.com’ (26 characters)

Product name

OCTET STRING

  • For IFE Ethernet interface for one circuit breaker (LV434001 or LV434010):

    ‘Ethernet interface for LV breakers’

  • For IFE Ethernet switchboard server (LV434002 or LV434011):

    ‘Ethernet interface for LV breakers + gateway’

  • For EIFE Ethernet interface (LV851001):

    ‘Embedded Ethernet interface for LV breakers’

Family

OCTET STRING

‘Gateway and server’

Range

OCTET STRING

‘Enerlin’X’

Model

OCTET STRING

IFE Ethernet interface’, ‘IFE/Gateway’, or ‘EIFE Ethernet interface’

Product ID

INT16U

Product ID of the core of IMU:

  • 17100 = IFE without gateway

  • 17101 = IFE with gateway

  • 17107 = EIFE

MAC Address of the IFE/EIFE Server

Address

Register

RW

Unit

Type

Range

Description

0x2E7D–

0x2E7F

11902–

11904

R

INT16U

MAC address of the IFE/EIFE interface coded over 3 registers (6 bytes) in hexadecimal.

Example: The MAC address 00:80:F4:02:12:34 (or 00-80-F4-02-12-34) is coded in hexadecimal as follows: 0080F4021234 (0x00 0x80 0xF4 0x02 0x12 0x34).

Manufacturing Date and Time

Address

Register

RW

Unit

Type

Range

Description

0x2E89–

0x2E8C

11914–

11917

R

DATETIME

Manufacturing date and time

IFE Interface Serial Number

The IFE interface serial number is composed of a maximum of 11 alphanumeric characters with the following format: PPYYWWDnnnn.

  • PP = plant code

  • YY = year of fabrication (0599)

  • WW = week of fabrication (0153)

  • D = day of fabrication (17)

  • nnnn = production number of the device on the day (00019999)

A read request of 6 registers is necessary to read the IFE interface serial number.

Address

Register

RW

Unit

Type

Range

Description

0x02E91

11922

R

OCTET STRING

‘PP’

0x02E92

11923

R

OCTET STRING

‘05’–‘99’

‘YY’

0x02E93

11924

R

OCTET STRING

‘01’–‘53’

‘WW’

0x02E94

11925

R

OCTET STRING

D: ‘1’–‘7’

n: ‘0’–‘9’

‘Dn’

0x02E95

11926

R

OCTET STRING

‘00’–‘99’

‘nn’

0x02E96

11927

R

OCTET STRING

‘0’–‘9’

‘n’ (the NULL character ends the serial number)

EIFE Interface Serial Number

The EIFE interface serial number is composed of a maximum of 16 alphanumeric characters with the following format: PPPPPPYYWWDLnnnn.

  • PPPPPP = plant code

  • YY = year of fabrication (0599)

  • WW = week of fabrication (0153)

  • D = day of fabrication (17)

  • L = Line or machine number (09 or az)

  • nnnn = production number of the device on the day (00019999)

A read request of 8 registers is necessary to read the EIFE interface serial number.

Address

Register

RW

Unit

Type

Range

Description

0x02E91–0x02E93

11922–11924

R

OCTET STRING

‘PPPPPP’

0x02E94

11925

R

OCTET STRING

‘05’–‘99’

‘YY’

0x02E95

11926

R

OCTET STRING

‘01’–‘53’

‘WW’

0x02E96

11927

R

OCTET STRING

D: ‘1’–’7’

L: ‘0’–’9’ or ‘a’–’z’

‘DL’

0x02E97–0x02E98

11928–11929

R

OCTET STRING

‘0000’–‘9999’

‘nnnn’

Modbus Parameters of the IFE Server

These parameters are valid for the IFE switchboard server only.

Address

Register

RW

Unit

Type

Range

Description

0x306F

12400

R

INT16U

Modbus address of IFE server (always 255)

0x3070

12401

R

INT16U

1–3

Modbus parity:

  • 1 = no parity

  • 2 = even parity (factory setting)

  • 3 = odd parity

0x3071

12402

R

INT16U

5–8

Modbus Baud rate:

  • 5 = 4800 Baud

  • 6 = 9600 Baud

  • 7 = 19,200 Baud (factory setting)

  • 8 = 38,400 Baud

0x3072

12403

R

INT16U

1,3,5

Number of stop bits:

  • 1 = Auto (factory setting)

  • 3 = 1 stop bit

  • 5 = 2 stop bits

Time Synchronization

Address

Register

RW

Unit

Type

Range

Description

0x3098–0x30B7

12441–12472

R

OCTET STRING

The type of source use for time synchronization:

  • ‘Auto–SNTP’

  • ‘Manual–Modbus’

  • ‘Manual–ULP’

  • ‘Manual–Webpage’

0x30B8–0x30BB

12473–12476

R

DATETIME

Date and time of last time synchronization

0x30BC–0x30BD

12477–12478

R

s

FLOAT32

Time since last time synchronization

0x30BE

12479

R

INT16U

0–2

Status of automatic time synchronization:

  • 0 = SNTP disabled

  • 1 = SNTP failed

  • 2 = SNTP succeeded

0x30BF

12480

R

INT16

SNTP fails count

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.